<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LCP11U67 and temperature reset in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP11U67-and-temperature-reset/m-p/534648#M10860</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbehlau on Fri May 22 01:32:25 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've noticed a big problem in some of my boards which are mounting LCP11U67 micros, with 48 pin. When I put them in their appropriate boxes, the heat generated (ambient temperature is around 30°C/40°C) some of the micro stopped. I'm using a watchdog, so the devices are restarted, but fails after 1-2 seconds again. After cool down, they work normally. The intern temperature sensor told me, the junction temperature is 85°C, when the problem occurred. The chip is specified for 105°C! The percentage of micro with this problem is low (2 devices from ~50 tested chips), but it is a big problem for me. If the lpc fails, the entire board, which all mounted parts, is completely worthless and can't be used in the field.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone ever noticed this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:36:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:36:50Z</dc:date>
    <item>
      <title>LCP11U67 and temperature reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP11U67-and-temperature-reset/m-p/534648#M10860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mbehlau on Fri May 22 01:32:25 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've noticed a big problem in some of my boards which are mounting LCP11U67 micros, with 48 pin. When I put them in their appropriate boxes, the heat generated (ambient temperature is around 30°C/40°C) some of the micro stopped. I'm using a watchdog, so the devices are restarted, but fails after 1-2 seconds again. After cool down, they work normally. The intern temperature sensor told me, the junction temperature is 85°C, when the problem occurred. The chip is specified for 105°C! The percentage of micro with this problem is low (2 devices from ~50 tested chips), but it is a big problem for me. If the lpc fails, the entire board, which all mounted parts, is completely worthless and can't be used in the field.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone ever noticed this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP11U67-and-temperature-reset/m-p/534648#M10860</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: LCP11U67 and temperature reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP11U67-and-temperature-reset/m-p/534649#M10861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lix on Tue May 26 07:00:21 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you find the solution to your problem? We have the same issue with the LPC11E67. If we run them at 48 MHz, they hang-up at temperatures over 75 degrees (it depends on the chip, some hang at 75, other over 80 degrees). If the clock is reduced to 36 MHz, no more hang-ups, even at 100 degrees Celsius!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this a known issue maybe? The errata says nothing about it.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP11U67-and-temperature-reset/m-p/534649#M10861</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:36:51Z</dc:date>
    </item>
  </channel>
</rss>