<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: JTAG not working when oscilloscope is connected to CLK0</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534223#M10783</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this sounds weird. The CLK0 pin normally outputs a clock to the SDRAM, on this board it is used as clock output for the SD-card. But after reset it is configured for EMC_CLK0 function.&lt;/P&gt;&lt;P&gt;The pin 45 of CLK0 is not close to the JTAG pins, so a connection between these pins could only be caused by an external shortcut. Maybe test with an ohm-meter for shortcust between CLK0 and other pins, especially the ones from JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;NXP Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Aug 2016 09:57:50 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2016-08-03T09:57:50Z</dc:date>
    <item>
      <title>JTAG not working when oscilloscope is connected to CLK0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534220#M10780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using LPC4337with J-link debuger in IAR ide. I noticed that when i connect oscilloscope to the CLK0 pin i'm not able to download the software into CPU and debug, I also see the square signal on CLK0 pin during connection. It seems that CLK0 is internally routed to JTAG pins. Why this is happening? The oscolloscope is 1Mohm 15pF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Jul 2016 15:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534220#M10780</guid>
      <dc:creator>aurimaspaulausk</dc:creator>
      <dc:date>2016-07-24T15:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG not working when oscilloscope is connected to CLK0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534221#M10781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aurimas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using a NXP evaluation board? Could you tell us the complete part number being used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 16:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534221#M10781</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-07-26T16:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG not working when oscilloscope is connected to CLK0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534222#M10782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using non NXP manufactured board. It is from Waveshare. Here is the link to the board: &lt;A href="http://www.waveshare.com/open4337-c-package-a.htm"&gt;http://www.waveshare.com/open4337-c-package-a.htm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I noticed that it is enough to touche the CLK0 pin with the finger and the debug is not working.&lt;/P&gt;&lt;P&gt;I guess CLK0 is connected internally to some circuitry. Because i see signals during the debug on CLK0 pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 14:22:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534222#M10782</guid>
      <dc:creator>aurimaspaulausk</dc:creator>
      <dc:date>2016-07-28T14:22:32Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG not working when oscilloscope is connected to CLK0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534223#M10783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this sounds weird. The CLK0 pin normally outputs a clock to the SDRAM, on this board it is used as clock output for the SD-card. But after reset it is configured for EMC_CLK0 function.&lt;/P&gt;&lt;P&gt;The pin 45 of CLK0 is not close to the JTAG pins, so a connection between these pins could only be caused by an external shortcut. Maybe test with an ohm-meter for shortcust between CLK0 and other pins, especially the ones from JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;NXP Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2016 09:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/JTAG-not-working-when-oscilloscope-is-connected-to-CLK0/m-p/534223#M10783</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2016-08-03T09:57:50Z</dc:date>
    </item>
  </channel>
</rss>