<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programming LPC11U24 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534130#M10769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Paul on Fri Oct 04 08:31:21 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you using one of the example projects that are available on LPCware?&amp;nbsp; It is always best to try a simple "blinky" project to confirm the hardware is working correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The device boots using the internal RC oscillator, so if you are stuck in the bootloader, or if your code has caused a exception before it reaches the code which enables the crystal oscillator, you will not see anything on the crystal pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Make sure the ISP pin (PIO0_1) is high, or else you could enter ISP mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The checksum at memory location 0x1C must be valid.&amp;nbsp; FlashMagic should calculate the checksum and program this memory location, so this is probably not the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You will probably need to use a debugger to help you isolate the problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:33:56 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:33:56Z</dc:date>
    <item>
      <title>Programming LPC11U24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534129#M10768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nlcomputers on Fri Oct 04 08:11:54 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Good Afternoon,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am after a little advice, I have designed a circuit and had a PCB produced. The PCB is now populated with an LPC11U24/401 48pin and the required passives.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem comes after the device has been programmed (with FlashMagic), in that the code never seems to run.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Flash magic can successfully read the serial number and bootloader version. It also sends the program and can verify it. I have sent a simple program (set output high then low of port 0,15).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Oscilloscope sees nothing on the port, nor the crystal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone offer any advice or tests I can perform to help diagnose this issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534129#M10768</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: Programming LPC11U24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534130#M10769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Paul on Fri Oct 04 08:31:21 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you using one of the example projects that are available on LPCware?&amp;nbsp; It is always best to try a simple "blinky" project to confirm the hardware is working correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The device boots using the internal RC oscillator, so if you are stuck in the bootloader, or if your code has caused a exception before it reaches the code which enables the crystal oscillator, you will not see anything on the crystal pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Make sure the ISP pin (PIO0_1) is high, or else you could enter ISP mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The checksum at memory location 0x1C must be valid.&amp;nbsp; FlashMagic should calculate the checksum and program this memory location, so this is probably not the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You will probably need to use a debugger to help you isolate the problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534130#M10769</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Programming LPC11U24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534131#M10770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nlcomputers on Sun Oct 06 10:02:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for responding.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had some time to debug this issue today and it turned out to be a short between crystal capacitors! Remove this and everything operated as expected!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-LPC11U24/m-p/534131#M10770</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:33:57Z</dc:date>
    </item>
  </channel>
</rss>