<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Arduino code on LPC1347 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Arduino-code-on-LPC1347/m-p/533649#M10681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a &lt;A class="postlink" href="http://bit.ly/2a4sqCP"&gt;short video of LPCXpresso 1347 board running code from Arduino IDE&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Compiler and uploader are from LPCXpresso IDE installed on the same workstation. This is proof of concept which uses libraries that come with Arduino-XC (SPI, Serial, Wire, some Adafruit libs etc.).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial Monitor seems to have some issues with FTDI USB serial dongle I'm using, so I just used minicom to display serial data coming from the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 21:33:56 GMT</pubDate>
    <dc:creator>nidalp</dc:creator>
    <dc:date>2016-08-02T21:33:56Z</dc:date>
    <item>
      <title>Arduino code on LPC1347</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Arduino-code-on-LPC1347/m-p/533648#M10680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone interested running Arduino (generic) code, or using Arduino libraries (like Adafruit) on LPC13xx (or almost any other LPC), check this out: &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fbit.ly%2F2a4sqCP" rel="nofollow" target="_blank"&gt;Arduino-XC - LPC1347&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Very usable (UART, SPI, I2C, half a dozen of Adafruit libraries: ADXL345, BMP085, GFX/LCD, ST7735, TCS34725, LSM303) but still under heavy development.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 21:03:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Arduino-code-on-LPC1347/m-p/533648#M10680</guid>
      <dc:creator>nidalp</dc:creator>
      <dc:date>2016-07-22T21:03:59Z</dc:date>
    </item>
    <item>
      <title>Re: Arduino code on LPC1347</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Arduino-code-on-LPC1347/m-p/533649#M10681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a &lt;A class="postlink" href="http://bit.ly/2a4sqCP"&gt;short video of LPCXpresso 1347 board running code from Arduino IDE&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Compiler and uploader are from LPCXpresso IDE installed on the same workstation. This is proof of concept which uses libraries that come with Arduino-XC (SPI, Serial, Wire, some Adafruit libs etc.).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial Monitor seems to have some issues with FTDI USB serial dongle I'm using, so I just used minicom to display serial data coming from the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 21:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Arduino-code-on-LPC1347/m-p/533649#M10681</guid>
      <dc:creator>nidalp</dc:creator>
      <dc:date>2016-08-02T21:33:56Z</dc:date>
    </item>
  </channel>
</rss>