<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Question to AN10995</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-to-AN10995/m-p/530898#M10096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Lea on Sun Feb 14 09:16:38 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This application note explain for cortex M0 the vector table must use interrupt re-direct functions. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I look inside the example code ans could not unterstand where the bootloader use an interrupt function handler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In xmodem1k.c is define a function &lt;/SPAN&gt;&lt;I&gt;static void vTimerStart(uint32_t u32Periodms)&lt;/I&gt;&lt;SPAN&gt; and within the function&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;I&gt;vXmodem1k_Client&lt;/I&gt;&lt;SPAN&gt; the timer is start a few times.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But where is the timer handler, where send another poll? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I only found the interrupt re-direct function &lt;/SPAN&gt;&lt;I&gt;void TIMER32_0_IRQHandler(void)&lt;/I&gt;&lt;SPAN&gt; inside main.c&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:30:36 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:30:36Z</dc:date>
    <item>
      <title>Question to AN10995</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-to-AN10995/m-p/530898#M10096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Lea on Sun Feb 14 09:16:38 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This application note explain for cortex M0 the vector table must use interrupt re-direct functions. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I look inside the example code ans could not unterstand where the bootloader use an interrupt function handler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In xmodem1k.c is define a function &lt;/SPAN&gt;&lt;I&gt;static void vTimerStart(uint32_t u32Periodms)&lt;/I&gt;&lt;SPAN&gt; and within the function&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;I&gt;vXmodem1k_Client&lt;/I&gt;&lt;SPAN&gt; the timer is start a few times.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But where is the timer handler, where send another poll? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I only found the interrupt re-direct function &lt;/SPAN&gt;&lt;I&gt;void TIMER32_0_IRQHandler(void)&lt;/I&gt;&lt;SPAN&gt; inside main.c&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-to-AN10995/m-p/530898#M10096</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:30:36Z</dc:date>
    </item>
  </channel>
</rss>