<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックaccess SDMMC as a storage media from PC thru USB using LPC1800</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/access-SDMMC-as-a-storage-media-from-PC-thru-USB-using-LPC1800/m-p/530803#M10081</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ChewTP on Wed Oct 15 02:45:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi I need some help here . I would like to implement SDMMC as a Mass storage device media when connected to the PC . I am looking at the msc_ram and perish_sdmmc examples in the LPCOpen . Same examples that you are looking . I would like to implement read , write , change directory , rename in the SDMMC card when view from PC . &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think using the USBD ROM driver in the mass storage class , they only have translate_wr , translate_rd , verify ..etc but with just these two callback function , how can I implement those functionn like change directory , rename delete , copy ...etc&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe it can implement read and write but to use it like a normal storage device , it is more than just read and write . Any idea how to do that .&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:17:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:17:57Z</dc:date>
    <item>
      <title>access SDMMC as a storage media from PC thru USB using LPC1800</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/access-SDMMC-as-a-storage-media-from-PC-thru-USB-using-LPC1800/m-p/530803#M10081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ChewTP on Wed Oct 15 02:45:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi I need some help here . I would like to implement SDMMC as a Mass storage device media when connected to the PC . I am looking at the msc_ram and perish_sdmmc examples in the LPCOpen . Same examples that you are looking . I would like to implement read , write , change directory , rename in the SDMMC card when view from PC . &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think using the USBD ROM driver in the mass storage class , they only have translate_wr , translate_rd , verify ..etc but with just these two callback function , how can I implement those functionn like change directory , rename delete , copy ...etc&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe it can implement read and write but to use it like a normal storage device , it is more than just read and write . Any idea how to do that .&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/access-SDMMC-as-a-storage-media-from-PC-thru-USB-using-LPC1800/m-p/530803#M10081</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: access SDMMC as a storage media from PC thru USB using LPC1800</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/access-SDMMC-as-a-storage-media-from-PC-thru-USB-using-LPC1800/m-p/530804#M10082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JM_Romero on Tue Nov 18 10:18:38 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi ChewTP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;If you are looking for using the microcontroller, as a transparent device, such as when you connect it to the PC, your system detect the SD/MMC card as a card and nothing else, then I would recommend you to modify the example found in &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fsystem%2Ffiles%2FMicroSD%2520card.zip" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/system/files/MicroSD%20card.zip&lt;/A&gt;&lt;SPAN&gt;. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In this example the PC detects the usb0 as mass storage device, and usb1 as a sound interface. By removing the sound interface related libraries and code, you should be able to use the microcontroller as a card reader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;JM_Romero.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/access-SDMMC-as-a-storage-media-from-PC-thru-USB-using-LPC1800/m-p/530804#M10082</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:17:58Z</dc:date>
    </item>
  </channel>
</rss>