<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 	• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ACSafe10-axf-Error-L6220E-Load-region-LR-IROM1-size-57352-bytes/m-p/468643#M1</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;I just starting getting this linker error when adding new code to an existing LPC2132FBD64/01 project.&amp;nbsp; I believe it means there is no more code space available, is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Keil ARM Basic 4.1 and the target options are set as RO Memory area IROM1: 0x2000 len 0xE000.&amp;nbsp; Are these values correct for allotting all available code space?&lt;/P&gt;&lt;P&gt;Any suggestions for squeezing a bit more into this processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 May 2016 19:54:00 GMT</pubDate>
    <dc:creator>steve_young1</dc:creator>
    <dc:date>2016-05-31T19:54:00Z</dc:date>
    <item>
      <title>• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ACSafe10-axf-Error-L6220E-Load-region-LR-IROM1-size-57352-bytes/m-p/468643#M1</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;I just starting getting this linker error when adding new code to an existing LPC2132FBD64/01 project.&amp;nbsp; I believe it means there is no more code space available, is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Keil ARM Basic 4.1 and the target options are set as RO Memory area IROM1: 0x2000 len 0xE000.&amp;nbsp; Are these values correct for allotting all available code space?&lt;/P&gt;&lt;P&gt;Any suggestions for squeezing a bit more into this processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 May 2016 19:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ACSafe10-axf-Error-L6220E-Load-region-LR-IROM1-size-57352-bytes/m-p/468643#M1</guid>
      <dc:creator>steve_young1</dc:creator>
      <dc:date>2016-05-31T19:54:00Z</dc:date>
    </item>
  </channel>
</rss>