<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Linux Embedded ChallengeのトピックRe: SPI driver not working as expected on powerpc hardware platform (with yocto build system)</title>
    <link>https://community.nxp.com/t5/Linux-Embedded-Challenge/SPI-driver-not-working-as-expected-on-powerpc-hardware-platform/m-p/2378835#M137</link>
    <description>&lt;P&gt;It will be very helpful if you reply if you have suggestion.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jun 2026 08:59:14 GMT</pubDate>
    <dc:creator>bharatbhardava</dc:creator>
    <dc:date>2026-06-09T08:59:14Z</dc:date>
    <item>
      <title>SPI driver not working as expected on powerpc hardware platform (with yocto build system)</title>
      <link>https://community.nxp.com/t5/Linux-Embedded-Challenge/SPI-driver-not-working-as-expected-on-powerpc-hardware-platform/m-p/2378063#M136</link>
      <description>&lt;P&gt;Hello, all,&lt;BR /&gt;I have old build system with inbuild kernel (2.6.73.x) and my application successfully compiles and working on our custom Linux board(based on PowerPC architecture) fine.&lt;BR /&gt;Now we migrated to YOCTO build system where latest kernel (6.x.x) is there. Now I observed that SPI devices not working as expected(which was working with old build system).&lt;BR /&gt;I know there is lot of dynamics/parameter changed with big jump in kernel version(hench in SPI driver). I have put some delay in change mode and control chip select API, it improve somewhat but not successful.&lt;BR /&gt;I have tried with many experiment to change SPI controller parameter but not get succeed. I have got some help from internet but not resolved my issue. As per me it is timing related issue. But i don't know exact location where to fix.&lt;BR /&gt;So, if you faced this type or similar challenge then you can lead/help. I appreciate any suggestion/fix/help/direction.&lt;/P&gt;&lt;P&gt;Thank you&lt;BR /&gt;Bharat&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 05:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Linux-Embedded-Challenge/SPI-driver-not-working-as-expected-on-powerpc-hardware-platform/m-p/2378063#M136</guid>
      <dc:creator>bharatbhardava</dc:creator>
      <dc:date>2026-06-08T05:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: SPI driver not working as expected on powerpc hardware platform (with yocto build system)</title>
      <link>https://community.nxp.com/t5/Linux-Embedded-Challenge/SPI-driver-not-working-as-expected-on-powerpc-hardware-platform/m-p/2378835#M137</link>
      <description>&lt;P&gt;It will be very helpful if you reply if you have suggestion.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jun 2026 08:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Linux-Embedded-Challenge/SPI-driver-not-working-as-expected-on-powerpc-hardware-platform/m-p/2378835#M137</guid>
      <dc:creator>bharatbhardava</dc:creator>
      <dc:date>2026-06-09T08:59:14Z</dc:date>
    </item>
  </channel>
</rss>