<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1993218#M960</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From the block diagram, you can see that there is a DCB brake module, which can discharge the regeneration energy to a power resistor and becomes heat.&lt;/P&gt;
&lt;P&gt;But I suppose it can not power the main AC power with the regeneration energy, in other words, this is a motor solution instead of a generator.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1731462854253.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310148i397ADCCD67A3A303/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1731462854253.png" alt="xiangjun_rong_0-1731462854253.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Wed, 13 Nov 2024 01:58:09 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-11-13T01:58:09Z</dc:date>
    <item>
      <title>MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1992541#M959</link>
      <description>&lt;P&gt;I worked on ACIM control using HVP-MC3PH development kit using&amp;nbsp;MCRSP_ACIM_V1.2.0 ACIM reference solution package.&lt;/P&gt;&lt;P&gt;I want to check the regeneration of induction motor.I tried a lot in different way. But no regeneration happen.&lt;/P&gt;&lt;P&gt;Is it possible in this platform?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 06:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1992541#M959</guid>
      <dc:creator>Mathupandi</dc:creator>
      <dc:date>2024-11-12T06:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1993218#M960</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From the block diagram, you can see that there is a DCB brake module, which can discharge the regeneration energy to a power resistor and becomes heat.&lt;/P&gt;
&lt;P&gt;But I suppose it can not power the main AC power with the regeneration energy, in other words, this is a motor solution instead of a generator.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1731462854253.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310148i397ADCCD67A3A303/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1731462854253.png" alt="xiangjun_rong_0-1731462854253.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 01:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1993218#M960</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-13T01:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1993455#M961</link>
      <description>I put the bulb in DCB brake terminal. But there is no glow happen.&lt;BR /&gt;I supply the power board with Battery pack and run the motor(motor connect with flywheel) at high RPM then suddenly reduce the RPM.&lt;BR /&gt;As per induction motor principle, the motor run above the synchronous speed the regeneration occurs.&lt;BR /&gt;But there is no voltage rise in the DC bus.&lt;BR /&gt;Is there any control mechanism handled in program for blocking the regeneration?</description>
      <pubDate>Wed, 13 Nov 2024 07:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1993455#M961</guid>
      <dc:creator>Mathupandi</dc:creator>
      <dc:date>2024-11-13T07:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1997653#M968</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I copy the circuit from the schematics of HVP, when the Brake_gate logic is high, the Q4 MOSFET will turn on, you can replace D21 diode with a bulb, the bulb will light.&lt;/P&gt;
&lt;P&gt;The chip tests the voltage of DCB_brake_voltage_sense signal, when it exceeds a threshold, the Brake_gate will be high with firmware&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1732074198744.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/311368i67AA4F98672AE40B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1732074198744.png" alt="xiangjun_rong_0-1732074198744.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 03:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1997653#M968</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-20T03:49:08Z</dc:date>
    </item>
    <item>
      <title>Re: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1997997#M969</link>
      <description>Is it necessary to replace the diode?&lt;BR /&gt;I have connected the bulb across the diode(between brake_res_2 and brake_res_1). But not glow.&lt;BR /&gt;&lt;BR /&gt;Note: I have already check this circuit by changing the threshold voltage value(below DC bus voltage) in firmware without connecting motor. The bulb will glow. But checking for regeneration the Q4 is not turn on.</description>
      <pubDate>Wed, 20 Nov 2024 11:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/1997997#M969</guid>
      <dc:creator>Mathupandi</dc:creator>
      <dc:date>2024-11-20T11:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCRSP_ACIM_V1.2.0 ACIM reference solution</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/2003458#M970</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I do not think you need to remove the diode. You just need to connect the bulb in parallel with the diode, it is okay.&lt;/P&gt;
&lt;P&gt;When the voltage of DCB_brake_voltage_sense node exceeds a threshold, the Brake_gate GPIO pin is set to high by software, the Q4 will turn on, the bulb will light.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 07:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCRSP-ACIM-V1-2-0-ACIM-reference-solution/m-p/2003458#M970</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-28T07:28:30Z</dc:date>
    </item>
  </channel>
</rss>