<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Motor Control with FRDM-GD3000EVB in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Motor-Control-with-FRDM-GD3000EVB/m-p/1472945#M858</link>
    <description>&lt;P&gt;I am designing a brushless DC motor control electronics assembly, and I am conducting bench testing with a hardware setup consisting of a FRDM-MC LVMTR, a FRDM-KV31F, a FRDM-GD3000EVB, and a FRDM-PWRSTG1EVB. I'd like to use MCUXpresso for the IDE and find a project to instantiate on the hardware and evaluate the motor performance, but I have not met with success.&lt;/P&gt;&lt;P&gt;Right now I'm trying to use I'm using the project frdmkv31f_mc_bldc, but all I get is a blinking red D4 LED, and no motor movement.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm the electronics hardware engineer on the project (very little software experience), and I only need to spin the motor (under any type of control), verify that the hardware and IDE toolchain will meet our needs, and then I can pass it all along to our software engineers.&lt;/P&gt;&lt;P&gt;Their IDE of choice is MCUXpresso.&lt;/P&gt;&lt;P&gt;Can anyone provide guidance? Thanks!&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jun 2022 14:19:49 GMT</pubDate>
    <dc:creator>DBanks60</dc:creator>
    <dc:date>2022-06-13T14:19:49Z</dc:date>
    <item>
      <title>Motor Control with FRDM-GD3000EVB</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Motor-Control-with-FRDM-GD3000EVB/m-p/1472945#M858</link>
      <description>&lt;P&gt;I am designing a brushless DC motor control electronics assembly, and I am conducting bench testing with a hardware setup consisting of a FRDM-MC LVMTR, a FRDM-KV31F, a FRDM-GD3000EVB, and a FRDM-PWRSTG1EVB. I'd like to use MCUXpresso for the IDE and find a project to instantiate on the hardware and evaluate the motor performance, but I have not met with success.&lt;/P&gt;&lt;P&gt;Right now I'm trying to use I'm using the project frdmkv31f_mc_bldc, but all I get is a blinking red D4 LED, and no motor movement.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm the electronics hardware engineer on the project (very little software experience), and I only need to spin the motor (under any type of control), verify that the hardware and IDE toolchain will meet our needs, and then I can pass it all along to our software engineers.&lt;/P&gt;&lt;P&gt;Their IDE of choice is MCUXpresso.&lt;/P&gt;&lt;P&gt;Can anyone provide guidance? Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 14:19:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Motor-Control-with-FRDM-GD3000EVB/m-p/1472945#M858</guid>
      <dc:creator>DBanks60</dc:creator>
      <dc:date>2022-06-13T14:19:49Z</dc:date>
    </item>
    <item>
      <title>Re: Motor Control with FRDM-GD3000EVB</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Motor-Control-with-FRDM-GD3000EVB/m-p/1475602#M863</link>
      <description>&lt;P&gt;Hello Dick Banks,&lt;/P&gt;
&lt;P&gt;I see that you have another case with the same question, I will follow up on this last one that I mention.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 00:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Motor-Control-with-FRDM-GD3000EVB/m-p/1475602#M863</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-06-17T00:46:19Z</dc:date>
    </item>
  </channel>
</rss>