<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: Convert KMS to MCAT project</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002911#M819</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello vegard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had the same issue with KMS discontinue. I do not believe there is a simple conversion from KMS to the MCAT/FREEMASTER environment.&lt;/P&gt;&lt;P&gt;I am afraid you have to put some effort in AN12374 to get it working. I alos started agian with AN12374 and it worked pretty well even there are some &lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;teething problems. Unfortunatly I have no experiance with hall start.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I have now a version running with sensored torque controll and are working on a sensorless torque controll version.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;Conserning you parameters I would use MCAT/FREEMASTER to characterize your motor and regulator again. Relevant MCAT/FREEMASTER&amp;nbsp; files are included in AN12374. &lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I only had some issues when using the whole at 20kHz PWM but at 10kHz it is working fine.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I have no idea why your motor stops form startup to spin other than that you parameters are not correct causing&amp;nbsp;the observer not correct initializing or maybe an overcurrent deu to a to high startup current.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;Best regards Peter&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Nov 2019 09:08:52 GMT</pubDate>
    <dc:creator>petersch</dc:creator>
    <dc:date>2019-11-18T09:08:52Z</dc:date>
    <item>
      <title>Convert KMS to MCAT project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002910#M818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've nearly finished developing an application with custom HW+FW based on Kinetis Motor Suite, and before moving onto production of larger quantities I see now that KMS support is discontinued.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;AN12374&lt;SPAN&gt;&amp;nbsp;package and managed to get a running project fairly quickly using the MCAT tool. However, I'm struggling with getting the motor to run properly, for instance the motor stops when transitioning from startup to spin. Is there any way to easily convert the parameters used in the KMS project to similar parameters used by MCAT, or c&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;ould you assist me in converting my project?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;The MCU I'm using is&amp;nbsp;MKV31F256VLH12P, and KMS project is sensorless hall start.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, will you add support for field weakening operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Nov 2019 08:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002910#M818</guid>
      <dc:creator>vegard</dc:creator>
      <dc:date>2019-11-18T08:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: Convert KMS to MCAT project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002911#M819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello vegard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had the same issue with KMS discontinue. I do not believe there is a simple conversion from KMS to the MCAT/FREEMASTER environment.&lt;/P&gt;&lt;P&gt;I am afraid you have to put some effort in AN12374 to get it working. I alos started agian with AN12374 and it worked pretty well even there are some &lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;teething problems. Unfortunatly I have no experiance with hall start.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I have now a version running with sensored torque controll and are working on a sensorless torque controll version.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;Conserning you parameters I would use MCAT/FREEMASTER to characterize your motor and regulator again. Relevant MCAT/FREEMASTER&amp;nbsp; files are included in AN12374. &lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I only had some issues when using the whole at 20kHz PWM but at 10kHz it is working fine.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;I have no idea why your motor stops form startup to spin other than that you parameters are not correct causing&amp;nbsp;the observer not correct initializing or maybe an overcurrent deu to a to high startup current.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN title=""&gt;Best regards Peter&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Nov 2019 09:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002911#M819</guid>
      <dc:creator>petersch</dc:creator>
      <dc:date>2019-11-18T09:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: Convert KMS to MCAT project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002912#M820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I find the tuning process in MCAT much more tedious than with KMS, and I wonder if I should develop on a different platform instead..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 06:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002912#M820</guid>
      <dc:creator>vegard</dc:creator>
      <dc:date>2019-11-19T06:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: Convert KMS to MCAT project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002913#M821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vegard,&lt;/P&gt;&lt;P&gt;Yes if your HW differs a lot from any of the NXP/Freescale development platforms it is wise to use one of these development platforms first. I used the FRDM-KV31F + FRDM-MC-LVPMSM to start with (same as for KMS) and that worked fine without any problems. My own HW is based on this platform with some changes and so only a few addaptions were needed to get it all running including MCAT. Changing to a different CPU is for later on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 16:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Convert-KMS-to-MCAT-project/m-p/1002913#M821</guid>
      <dc:creator>petersch</dc:creator>
      <dc:date>2019-11-19T16:09:17Z</dc:date>
    </item>
  </channel>
</rss>