<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックKV31F with KMS Not Working!!</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KV31F-with-KMS-Not-Working/m-p/995764#M816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I am trying to use KMS 1.1.0 with KV31F.&lt;/P&gt;&lt;P&gt;Initially, I flashed KV31F with KDS 3.2.0 demo program (PMSM_ref_sol). It worked. I was able to control the motor speed using freemaster and SW2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I try to use KMS with KV31F, it says it could not verify the communication over the UART port.&amp;nbsp;&lt;/P&gt;&lt;P&gt;(The same UART port worked perfectly for KDS program).&lt;/P&gt;&lt;P&gt;Can anyone tell me what's the problem?&lt;/P&gt;&lt;P&gt;I went through the community and it mentioned the KMS image not being flashed properly onto the KV31F board.&lt;/P&gt;&lt;P&gt;How do I check it?&lt;/P&gt;&lt;P&gt;I tried all the troubleshooting. Putting into bootloader and open&amp;nbsp;SDA again. But it still does not work. Two boards, I have the same error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Jan 2020 06:45:44 GMT</pubDate>
    <dc:creator>trialaccount12</dc:creator>
    <dc:date>2020-01-12T06:45:44Z</dc:date>
    <item>
      <title>KV31F with KMS Not Working!!</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KV31F-with-KMS-Not-Working/m-p/995764#M816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I am trying to use KMS 1.1.0 with KV31F.&lt;/P&gt;&lt;P&gt;Initially, I flashed KV31F with KDS 3.2.0 demo program (PMSM_ref_sol). It worked. I was able to control the motor speed using freemaster and SW2.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I try to use KMS with KV31F, it says it could not verify the communication over the UART port.&amp;nbsp;&lt;/P&gt;&lt;P&gt;(The same UART port worked perfectly for KDS program).&lt;/P&gt;&lt;P&gt;Can anyone tell me what's the problem?&lt;/P&gt;&lt;P&gt;I went through the community and it mentioned the KMS image not being flashed properly onto the KV31F board.&lt;/P&gt;&lt;P&gt;How do I check it?&lt;/P&gt;&lt;P&gt;I tried all the troubleshooting. Putting into bootloader and open&amp;nbsp;SDA again. But it still does not work. Two boards, I have the same error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jan 2020 06:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KV31F-with-KMS-Not-Working/m-p/995764#M816</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2020-01-12T06:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: KV31F with KMS Not Working!!</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KV31F-with-KMS-Not-Working/m-p/995765#M817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please see the announcement about KMS.&amp;nbsp;&lt;A href="https://community.nxp.com/community/general-purpose-mcus/kinetis/kms"&gt;https://community.nxp.com/community/general-purpose-mcus/kinetis/kms&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 17:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KV31F-with-KMS-Not-Working/m-p/995765#M817</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2020-01-13T17:56:07Z</dc:date>
    </item>
  </channel>
</rss>