<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: KMS_TICK-&amp;gt;CYCCNT Not Counting when Debugger Not Connected</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800656#M587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Adam,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. I seem to have fixed the issue by moving&amp;nbsp;StartProfiler() under EnableGlobalIRQ(). I am a little uncomfortable about this because I am unsure as to why moving the Profiler under the IRQ enable would resolve this issue, as you do not run this sequence of events in your KMS project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is the sequence of events in which the profiler was hanging each time without the debugger connected:&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Init Platform Independent Motor Commander Core */&lt;BR /&gt; DRV_init(&amp;amp;flashSysParams);&lt;/P&gt;&lt;P&gt;/* Enable the Profile to be free running */&lt;BR /&gt; &lt;STRONG&gt;StartProfiler();&lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt; /* Enable UART ISRs */&lt;BR /&gt; NVIC_EnableIRQ(UART1_RX_TX_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_RX_TX_IRQn, 14);&lt;BR /&gt; NVIC_EnableIRQ(UART1_ERR_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_ERR_IRQn, 14);&lt;/P&gt;&lt;P&gt;focPwmDecimation = flashSysParamsHeader.FocPwmDecimation; /*!&amp;lt; PWM to Fast ISR Decimation */&lt;BR /&gt; fastTicksPerSlowTick = flashSysParamsHeader.fastTicksPerSlowTick; /*!&amp;lt; Fast to Slow ISR Decimation */&lt;/P&gt;&lt;P&gt;/* Enable Global interrupts */&lt;BR /&gt; EnableGlobalIRQ(ui32PrimaskReg);&lt;/P&gt;&lt;P&gt;/* Install handler for ADC1 (conversion complete) interrupt */&lt;BR /&gt; NVIC_EnableIRQ(ADC1_IRQn); /* enable ADC1 interrupt */&lt;BR /&gt; NVIC_SetPriority(ADC1_IRQn, 12);&lt;/P&gt;&lt;P&gt;/* Enable PDB0 ISR */&lt;BR /&gt; NVIC_EnableIRQ(PDB0_IRQn);&lt;BR /&gt; NVIC_SetPriority(PDB0_IRQn, 13);&lt;/P&gt;&lt;P&gt;/* Use the SWI IRQ to trigger the slow tick routine */&lt;BR /&gt; NVIC_EnableIRQ(SWI_IRQn);&lt;BR /&gt; NVIC_SetPriority(SWI_IRQn, 15);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I changed this to the following, and not the profiler starts every time without a problem:&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Init Platform Independent Motor Commander Core */&lt;BR /&gt; DRV_init(&amp;amp;flashSysParams);&lt;/P&gt;&lt;P&gt;/* Enable UART ISRs */&lt;BR /&gt; NVIC_EnableIRQ(UART1_RX_TX_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_RX_TX_IRQn, 14);&lt;BR /&gt; NVIC_EnableIRQ(UART1_ERR_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_ERR_IRQn, 14);&lt;/P&gt;&lt;P&gt;focPwmDecimation = flashSysParamsHeader.FocPwmDecimation; /*!&amp;lt; PWM to Fast ISR Decimation */&lt;BR /&gt; fastTicksPerSlowTick = flashSysParamsHeader.fastTicksPerSlowTick; /*!&amp;lt; Fast to Slow ISR Decimation */&lt;/P&gt;&lt;P&gt;/* Enable Global interrupts */&lt;BR /&gt; EnableGlobalIRQ(ui32PrimaskReg);&lt;/P&gt;&lt;P&gt;/* Enable the Profile to be free running */&lt;BR /&gt; &lt;STRONG&gt;StartProfiler();&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Install handler for ADC1 (conversion complete) interrupt */&lt;BR /&gt; NVIC_EnableIRQ(ADC1_IRQn); /* enable ADC1 interrupt */&lt;BR /&gt; NVIC_SetPriority(ADC1_IRQn, 12);&lt;/P&gt;&lt;P&gt;/* Enable PDB0 ISR */&lt;BR /&gt; NVIC_EnableIRQ(PDB0_IRQn);&lt;BR /&gt; NVIC_SetPriority(PDB0_IRQn, 13);&lt;/P&gt;&lt;P&gt;/* Use the SWI IRQ to trigger the slow tick routine */&lt;BR /&gt; NVIC_EnableIRQ(SWI_IRQn);&lt;BR /&gt; NVIC_SetPriority(SWI_IRQn, 15);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jul 2018 16:54:58 GMT</pubDate>
    <dc:creator>derekcook</dc:creator>
    <dc:date>2018-07-13T16:54:58Z</dc:date>
    <item>
      <title>KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800654#M585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having a strange problem that I am curious if you have seen or not, and if you know what may be causing it. In my Sensorless Velocity Project, when the debugger is not connected,&amp;nbsp;GetProfilerCycles() returns zero. This works fine when the debugger is connected, and in my sensored project. I was just wondering if maybe something keeps resetting this. Have you seen this before?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Derek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2018 19:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800654#M585</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-07-11T19:09:45Z</dc:date>
    </item>
    <item>
      <title>Re: KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800655#M586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't say that I've seen this before. We leverage the&amp;nbsp;DWT for this functionality. So I'm not sure what is going on there.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Take a look at the MCU documentation and ARM documentation (&lt;A class="link-titled" href="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0439b/BIIFBHIF.html" title="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0439b/BIIFBHIF.html"&gt;ARM Information Center&lt;/A&gt;&amp;nbsp;)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jul 2018 02:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800655#M586</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-07-13T02:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800656#M587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Adam,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. I seem to have fixed the issue by moving&amp;nbsp;StartProfiler() under EnableGlobalIRQ(). I am a little uncomfortable about this because I am unsure as to why moving the Profiler under the IRQ enable would resolve this issue, as you do not run this sequence of events in your KMS project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is the sequence of events in which the profiler was hanging each time without the debugger connected:&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Init Platform Independent Motor Commander Core */&lt;BR /&gt; DRV_init(&amp;amp;flashSysParams);&lt;/P&gt;&lt;P&gt;/* Enable the Profile to be free running */&lt;BR /&gt; &lt;STRONG&gt;StartProfiler();&lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt; /* Enable UART ISRs */&lt;BR /&gt; NVIC_EnableIRQ(UART1_RX_TX_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_RX_TX_IRQn, 14);&lt;BR /&gt; NVIC_EnableIRQ(UART1_ERR_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_ERR_IRQn, 14);&lt;/P&gt;&lt;P&gt;focPwmDecimation = flashSysParamsHeader.FocPwmDecimation; /*!&amp;lt; PWM to Fast ISR Decimation */&lt;BR /&gt; fastTicksPerSlowTick = flashSysParamsHeader.fastTicksPerSlowTick; /*!&amp;lt; Fast to Slow ISR Decimation */&lt;/P&gt;&lt;P&gt;/* Enable Global interrupts */&lt;BR /&gt; EnableGlobalIRQ(ui32PrimaskReg);&lt;/P&gt;&lt;P&gt;/* Install handler for ADC1 (conversion complete) interrupt */&lt;BR /&gt; NVIC_EnableIRQ(ADC1_IRQn); /* enable ADC1 interrupt */&lt;BR /&gt; NVIC_SetPriority(ADC1_IRQn, 12);&lt;/P&gt;&lt;P&gt;/* Enable PDB0 ISR */&lt;BR /&gt; NVIC_EnableIRQ(PDB0_IRQn);&lt;BR /&gt; NVIC_SetPriority(PDB0_IRQn, 13);&lt;/P&gt;&lt;P&gt;/* Use the SWI IRQ to trigger the slow tick routine */&lt;BR /&gt; NVIC_EnableIRQ(SWI_IRQn);&lt;BR /&gt; NVIC_SetPriority(SWI_IRQn, 15);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I changed this to the following, and not the profiler starts every time without a problem:&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Init Platform Independent Motor Commander Core */&lt;BR /&gt; DRV_init(&amp;amp;flashSysParams);&lt;/P&gt;&lt;P&gt;/* Enable UART ISRs */&lt;BR /&gt; NVIC_EnableIRQ(UART1_RX_TX_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_RX_TX_IRQn, 14);&lt;BR /&gt; NVIC_EnableIRQ(UART1_ERR_IRQn);&lt;BR /&gt; NVIC_SetPriority(UART1_ERR_IRQn, 14);&lt;/P&gt;&lt;P&gt;focPwmDecimation = flashSysParamsHeader.FocPwmDecimation; /*!&amp;lt; PWM to Fast ISR Decimation */&lt;BR /&gt; fastTicksPerSlowTick = flashSysParamsHeader.fastTicksPerSlowTick; /*!&amp;lt; Fast to Slow ISR Decimation */&lt;/P&gt;&lt;P&gt;/* Enable Global interrupts */&lt;BR /&gt; EnableGlobalIRQ(ui32PrimaskReg);&lt;/P&gt;&lt;P&gt;/* Enable the Profile to be free running */&lt;BR /&gt; &lt;STRONG&gt;StartProfiler();&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/* Install handler for ADC1 (conversion complete) interrupt */&lt;BR /&gt; NVIC_EnableIRQ(ADC1_IRQn); /* enable ADC1 interrupt */&lt;BR /&gt; NVIC_SetPriority(ADC1_IRQn, 12);&lt;/P&gt;&lt;P&gt;/* Enable PDB0 ISR */&lt;BR /&gt; NVIC_EnableIRQ(PDB0_IRQn);&lt;BR /&gt; NVIC_SetPriority(PDB0_IRQn, 13);&lt;/P&gt;&lt;P&gt;/* Use the SWI IRQ to trigger the slow tick routine */&lt;BR /&gt; NVIC_EnableIRQ(SWI_IRQn);&lt;BR /&gt; NVIC_SetPriority(SWI_IRQn, 15);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jul 2018 16:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800656#M587</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-07-13T16:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800657#M588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can take a peak at the StartProfiler function call. It merely configures the DWT hardware on the MCU. So moving it shouldn't have any impact. It is possible we did something wrong in the reference project with respect to the correct location.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 11:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800657#M588</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-07-17T11:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800658#M589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Moving the StartProfiler() around does not make sense to me. I'm not sure why it would&amp;nbsp;start any better after the EnableGlobalIRQ(). I'm afraid the issue may still be present, just not as prevalent as it was. I have not seen the issue since Friday, however.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the StartProfiler() function to another post online, and it seems to match pretty well as to what the other person was doing:&amp;nbsp;&lt;A class="link-titled" href="https://mcuoneclipse.com/2017/01/30/cycle-counting-on-arm-cortex-m-with-dwt/" title="https://mcuoneclipse.com/2017/01/30/cycle-counting-on-arm-cortex-m-with-dwt/"&gt;Cycle Counting on ARM Cortex-M with DWT | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the StartProfiler() it looks like the correct register is being written to enable the DEMCR (Debug Exception and Monitor Control Register).&lt;/P&gt;&lt;P&gt;The Control Register is being written to 1 to enable the cycle counter, and you're resetting the Cycle Counter.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did notice the KMS order of events was different than this online post however. I wonder if resetting the cycle counter after enabling it could maybe cause some inconsistency? I also noticed that when setting the control bit a '=' is used instead of '|='. I'm not sure if this would cause a problem either.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently StartProfiler() looks like this:&amp;nbsp;&lt;/P&gt;&lt;P&gt;static inline void StartProfiler(void)&lt;BR /&gt;{&lt;BR /&gt; CLOCK_ENABLE_KMS_TICK;&lt;/P&gt;&lt;P&gt;KMS_TICK-&amp;gt;CTRL = DWT_CTRL_CYCCNTENA_Msk;&amp;nbsp;&lt;/P&gt;&lt;P&gt;KMS_TICK-&amp;gt;CYCCNT = 0;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example online did this:&amp;nbsp;&lt;/P&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;KIN1_InitCycleCounter(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* enable DWT hardware */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;KIN1_ResetCycleCounter(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* reset cycle counter */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;KIN1_EnableCycleCounter(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* start counting */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;foo(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* call function and count cycles */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;cycles = KIN1_GetCycleCounter(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* get cycle counter */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: black !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;KIN1_DisableCycleCounter(); &lt;/CODE&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;/* disable counting if not used any more */&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;CODE class="" style="color: #008200 !important; background: none !important; border: 0px !important; font-weight: normal !important; margin: 0px !important; padding: 0px !important;"&gt;&amp;nbsp;&lt;/CODE&gt;&lt;/DIV&gt;&lt;DIV class="" style="color: #373737; background: none white !important; border: 0px !important; margin: 0px !important; padding: 0px 1em !important;"&gt;&lt;P style="color: #3d3d3d;"&gt;I wonder if start profiler should look like this - I'm just not sure if resetting the CYCCNT after enabling could cause the CYCCNT to get stuck at 0?&lt;/P&gt;&lt;P&gt;static inline void StartProfiler(void)&lt;BR /&gt;{&lt;BR /&gt; CLOCK_ENABLE_KMS_TICK;&lt;/P&gt;&lt;P&gt;KMS_TICK-&amp;gt;CYCCNT = 0;&lt;/P&gt;&lt;P&gt;KMS_TICK-&amp;gt;CTRL |= DWT_CTRL_CYCCNTENA_Msk;&lt;BR /&gt;}&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 16:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800658#M589</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-07-17T16:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: KMS_TICK-&gt;CYCCNT Not Counting when Debugger Not Connected</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800659#M590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could switch out the code and see if that resolves the issue. On the reference hardware the debugger isn't being used, and the mcu boots from flash. So I'm not sure why it works there but not on your board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 02:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/KMS-TICK-gt-CYCCNT-Not-Counting-when-Debugger-Not-Connected/m-p/800659#M590</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-07-18T02:57:43Z</dc:date>
    </item>
  </channel>
</rss>