<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: Speed Controller Current Limit Setting</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798470#M584</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Adam, That is what I needed to know.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jul 2018 19:01:13 GMT</pubDate>
    <dc:creator>derekcook</dc:creator>
    <dc:date>2018-07-11T19:01:13Z</dc:date>
    <item>
      <title>Speed Controller Current Limit Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798468#M582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the user guide, it states the motor rated current is used to determine the limit of the current out of the speed controller. Is this correct? If I want to run my system at 3x rated, then I have to set my rated motor current to 300% of rated?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Derek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2018 19:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798468#M582</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-07-10T19:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: Speed Controller Current Limit Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798469#M583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS defines the maximum commandable current to be the rated current of the motor. The current reference comes from the speed controller and so its output&amp;nbsp;limit will be the maximum commandable current in the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change the maximum and minimum values for the speed controller output limit programatically by modifying the variables:&lt;/P&gt;&lt;P&gt;user.command.IqRefMax &amp;amp;&amp;nbsp;&lt;SPAN&gt;user.command.&lt;/SPAN&gt;&lt;SPAN&gt;IqRefMin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These are Q24 variables that are normalized against FULL_SCALE_CURRENT. So ensure that your FULL_SCALE_CURRENT value is large enough to support your higher current.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2018 04:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798469#M583</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-07-11T04:18:00Z</dc:date>
    </item>
    <item>
      <title>Re: Speed Controller Current Limit Setting</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798470#M584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Adam, That is what I needed to know.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2018 19:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Speed-Controller-Current-Limit-Setting/m-p/798470#M584</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-07-11T19:01:13Z</dc:date>
    </item>
  </channel>
</rss>