<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor Suite中的主题 Re: How are the Current Regulator PI Constants Calculated?</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/How-are-the-Current-Regulator-PI-Constants-Calculated/m-p/793397#M565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just resolved my own question. If you enter the motor resistance, inductance and flux into the GUI, and then click store parameters to file, the GUI will calculate the kp, ki, kc and store them in the system.h file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jun 2018 20:26:34 GMT</pubDate>
    <dc:creator>derekcook</dc:creator>
    <dc:date>2018-06-18T20:26:34Z</dc:date>
    <item>
      <title>How are the Current Regulator PI Constants Calculated?</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/How-are-the-Current-Regulator-PI-Constants-Calculated/m-p/793396#M564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the Current Regulator Kp, and Ki constants are calculated from the Resistance, Inductance and Current Regulator Bandwidth from the GUI. Could you provide the calculations for these constants so that we do not need to use the automatic tuning to calculate them, we could instead use the motor datasheet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Derek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 20:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/How-are-the-Current-Regulator-PI-Constants-Calculated/m-p/793396#M564</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-06-18T20:00:17Z</dc:date>
    </item>
    <item>
      <title>Re: How are the Current Regulator PI Constants Calculated?</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/How-are-the-Current-Regulator-PI-Constants-Calculated/m-p/793397#M565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just resolved my own question. If you enter the motor resistance, inductance and flux into the GUI, and then click store parameters to file, the GUI will calculate the kp, ki, kc and store them in the system.h file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 20:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/How-are-the-Current-Regulator-PI-Constants-Calculated/m-p/793397#M565</guid>
      <dc:creator>derekcook</dc:creator>
      <dc:date>2018-06-18T20:26:34Z</dc:date>
    </item>
  </channel>
</rss>