<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Inertia SI Values in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Inertia-SI-Values/m-p/789955#M556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Vegard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to convert from A/(rpm/s) into SI you need to convert the electrical power (A) into mechanical power [N] using the torque equation:&lt;/P&gt;&lt;P&gt;Torque = 3/2 * Pp * Flux * Current&lt;/P&gt;&lt;P&gt;You also need to convert from rpm/s into elec rad / sec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This can be slightly tricky and it is important that your units are correctly aligned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 00:41:54 GMT</pubDate>
    <dc:creator>linestream-adam</dc:creator>
    <dc:date>2018-08-16T00:41:54Z</dc:date>
    <item>
      <title>Inertia SI Values</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Inertia-SI-Values/m-p/789954#M555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: medium;"&gt;The inertia values are measured through Kinetis Motor Suite and given in unit: [A/(rpm/s)]. How do I convert these values to SI units? I want to calculate the rotational energy.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 08:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Inertia-SI-Values/m-p/789954#M555</guid>
      <dc:creator>vegardlovvig</dc:creator>
      <dc:date>2018-08-15T08:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Inertia SI Values</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Inertia-SI-Values/m-p/789955#M556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Vegard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to convert from A/(rpm/s) into SI you need to convert the electrical power (A) into mechanical power [N] using the torque equation:&lt;/P&gt;&lt;P&gt;Torque = 3/2 * Pp * Flux * Current&lt;/P&gt;&lt;P&gt;You also need to convert from rpm/s into elec rad / sec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This can be slightly tricky and it is important that your units are correctly aligned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 00:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Inertia-SI-Values/m-p/789955#M556</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-08-16T00:41:54Z</dc:date>
    </item>
  </channel>
</rss>