<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: No load current vibration in Torque Control when I use KMS</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/No-load-current-vibration-in-Torque-Control-when-I-use-KMS/m-p/779015#M543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Banson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. That is fairly common for motors running in torque control with no load.&amp;nbsp; I would only expect it to be perfectly flat if you had the motor at stall.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. In the plot, it isn't showing the Q-axis reference.&amp;nbsp; It is plotting the speed controller output.&amp;nbsp;&amp;nbsp;In torque mode, the Q-axis reference is user.output.drvCommand.statorRefCurrent.q (Q24, BASE_CURRENT).&amp;nbsp; Which should be exactly equal to the value you put in the GUI, stored in&amp;nbsp;user.command.statorRefCurrent.q.&lt;/P&gt;&lt;P&gt;The D-axis reference is plotted against the right axis, which shows it is 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 May 2018 15:31:01 GMT</pubDate>
    <dc:creator>linestream-adam</dc:creator>
    <dc:date>2018-05-01T15:31:01Z</dc:date>
    <item>
      <title>No load current vibration in Torque Control when I use KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/No-load-current-vibration-in-Torque-Control-when-I-use-KMS/m-p/779014#M542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have 2 question about Cureent control of KMS as below:&lt;/P&gt;&lt;P&gt;1. When I test torque control with KMS (no load condition and bare shaft). I find Q-Aixs and D-Aixs current has a big vibration as the picture.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33229i0EB5BB6B694CFC86/image-size/large?v=v2&amp;amp;px=999" title="DQCurrents-2018-05-01T17-16-41.png" alt="DQCurrents-2018-05-01T17-16-41.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. I define Q-Aixs current is 0.20 A in torque control (as the below picture) . but in the above picture, Q-Aixs current reference is 0, and D-Aixs current reference is 0.17A. Why?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33153i8AFAE776A4A9997B/image-size/large?v=v2&amp;amp;px=999" title="Torque Control.PNG" alt="Torque Control.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 May 2018 09:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/No-load-current-vibration-in-Torque-Control-when-I-use-KMS/m-p/779014#M542</guid>
      <dc:creator>bansondou</dc:creator>
      <dc:date>2018-05-01T09:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: No load current vibration in Torque Control when I use KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/No-load-current-vibration-in-Torque-Control-when-I-use-KMS/m-p/779015#M543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Banson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. That is fairly common for motors running in torque control with no load.&amp;nbsp; I would only expect it to be perfectly flat if you had the motor at stall.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. In the plot, it isn't showing the Q-axis reference.&amp;nbsp; It is plotting the speed controller output.&amp;nbsp;&amp;nbsp;In torque mode, the Q-axis reference is user.output.drvCommand.statorRefCurrent.q (Q24, BASE_CURRENT).&amp;nbsp; Which should be exactly equal to the value you put in the GUI, stored in&amp;nbsp;user.command.statorRefCurrent.q.&lt;/P&gt;&lt;P&gt;The D-axis reference is plotted against the right axis, which shows it is 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 May 2018 15:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/No-load-current-vibration-in-Torque-Control-when-I-use-KMS/m-p/779015#M543</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-05-01T15:31:01Z</dc:date>
    </item>
  </channel>
</rss>