<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor Suite中的主题 Re: MCUXpresso problem opening KMS project</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766521#M492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With KMS 1.2 the only time you will need KDS is if you choose an ACIM motor type using the HVP (high voltage platform).&amp;nbsp; I don't this option is in very high demand as there are no-HVP KV31 or KV46 eval boards out to support that option yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 21:02:45 GMT</pubDate>
    <dc:creator>philip_drake</dc:creator>
    <dc:date>2018-02-22T21:02:45Z</dc:date>
    <item>
      <title>MCUXpresso problem opening KMS project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766519#M490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KMS that successfully characterized a motor, and I told it to export the project.&amp;nbsp; Now, the question is, am I supposed to be using MCUXpresso or Kinetis Design Studio to compile the project?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I use MCUXpresso I get the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MCUXpresso-KMS-Problem1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18570i5BF122C3AE804550/image-size/large?v=v2&amp;amp;px=999" role="button" title="MCUXpresso-KMS-Problem1.PNG" alt="MCUXpresso-KMS-Problem1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the question is, am I going down the correct path?&amp;nbsp; Or should I be using KDS?&amp;nbsp; And what do I do to fix this error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Paul Tan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 19:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766519#M490</guid>
      <dc:creator>PaulTan</dc:creator>
      <dc:date>2018-02-22T19:47:26Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso problem opening KMS project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766520#M491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nevermind, found solution - install SDK from&amp;nbsp;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, followed&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/video/mcuxpresso-ide-importing-mcuxpresso-sdk:MCUXPRESSO-IDE-IMPORTING-SDK" title="https://www.nxp.com/video/mcuxpresso-ide-importing-mcuxpresso-sdk:MCUXPRESSO-IDE-IMPORTING-SDK"&gt;MCUXpresso IDE - Importing MCUXpresso SDK|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Putting this up in case other people run into the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Paul Tan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 20:25:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766520#M491</guid>
      <dc:creator>PaulTan</dc:creator>
      <dc:date>2018-02-22T20:25:25Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso problem opening KMS project</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766521#M492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With KMS 1.2 the only time you will need KDS is if you choose an ACIM motor type using the HVP (high voltage platform).&amp;nbsp; I don't this option is in very high demand as there are no-HVP KV31 or KV46 eval boards out to support that option yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 21:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/MCUXpresso-problem-opening-KMS-project/m-p/766521#M492</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2018-02-22T21:02:45Z</dc:date>
    </item>
  </channel>
</rss>