<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: Low RPM application</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760130#M484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Randy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to manually modify the speeds in the generated MotionSequence.c file.&amp;nbsp; The VEL_PU normalizing macro accepts floating point inputs.&amp;nbsp; You can create your motion sequence in Motion Sequence Builder and than change the speeds manually in the MotionSequence.c file.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Apr 2018 00:34:24 GMT</pubDate>
    <dc:creator>linestream-adam</dc:creator>
    <dc:date>2018-04-04T00:34:24Z</dc:date>
    <item>
      <title>Low RPM application</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760127#M481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to operate my motor over a speed range that starts below 1 RPM.&amp;nbsp; Does the motor firmware and Kinetis Motor Suite support this range?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 14:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760127#M481</guid>
      <dc:creator>randyfields</dc:creator>
      <dc:date>2018-04-03T14:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: Low RPM application</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760128#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Randy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to operate on fractional RPM in KMS.&amp;nbsp; The GUI uses whole RPM since most people don't need the motor to spin that slowly. I will also caution you that this will only work reliably if you are running Sensored Velocity or Sensored Position control. Running below about 10% of rated speed is difficult when using Sensorless Velocity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've written up some instructions to get fractional rpm working through the GUI below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Make sure you have estimated the interia of your system.&lt;/LI&gt;&lt;LI&gt;Make sure the Speed Loop bandwidth is set fairly aggressively.&amp;nbsp; In my test, I maxed it out to 200 rad/s.&lt;/LI&gt;&lt;LI&gt;Open the Watch Window (View -&amp;gt; Watch Window)&lt;/LI&gt;&lt;LI&gt;Click the + button to add a variable&lt;/LI&gt;&lt;LI&gt;Navigate the tree to "user.command.targetSpeed" and click the arrows to add the variable&lt;/LI&gt;&lt;LI&gt;Click Play in the Watch Window to begin updating the value.&lt;/LI&gt;&lt;LI&gt;Type in your intended speed as the value for user.command.targetSpeed&lt;/LI&gt;&lt;LI&gt;In the KMS GUI, click Start/Stop Speed Control&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The speed value in the GUI will be 0 since they are not configured to display fractional numbers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 15:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760128#M482</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-04-03T15:40:32Z</dc:date>
    </item>
    <item>
      <title>Re: Low RPM application</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760129#M483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, that did allow me to operate below 1 RPM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way I can get the low RPM when I am using the Motion Planner?  I&lt;/P&gt;&lt;P&gt;am trying to set the plan velocity using the STPOSPLAN_addCfgTran()&lt;/P&gt;&lt;P&gt;function; regardless of the velocity I give it 1 RPM is as low as I can go.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Randy Fields&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Tue, Apr 3, 2018 at 11:41 AM, linestream-adamreynolds &amp;lt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 18:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760129#M483</guid>
      <dc:creator>randyfields</dc:creator>
      <dc:date>2018-04-03T18:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: Low RPM application</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760130#M484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Randy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to manually modify the speeds in the generated MotionSequence.c file.&amp;nbsp; The VEL_PU normalizing macro accepts floating point inputs.&amp;nbsp; You can create your motion sequence in Motion Sequence Builder and than change the speeds manually in the MotionSequence.c file.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 00:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Low-RPM-application/m-p/760130#M484</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-04-04T00:34:24Z</dc:date>
    </item>
  </channel>
</rss>