<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Spread Spectrum PWM in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Spread-Spectrum-PWM/m-p/758632#M480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Geoffrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS doesn't feature spread spectrum PWM by default.&amp;nbsp; You should be able to add support for this into KMS.&amp;nbsp; You would do this by replacing the SVPWM block with a new block of your own design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS sets up the PWMs to be center-aligned so that the ADC sample is taken in the middle of the PWM period.&amp;nbsp; So the ADC sample would occur in the same place regardless if the frequency is changing.&amp;nbsp;&amp;nbsp;In addition to modifying the frequency, you would also need to change the deadtime counter since the FlexTimer handles the deadtime insertion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think varying the PWM frequency by a few kHz would impact the control loops within KMS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2018 14:04:00 GMT</pubDate>
    <dc:creator>linestream-adam</dc:creator>
    <dc:date>2018-01-03T14:04:00Z</dc:date>
    <item>
      <title>Spread Spectrum PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Spread-Spectrum-PWM/m-p/758631#M479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the KMS support spread spectrum PWM?&amp;nbsp; &amp;nbsp;Has anyone attempted to modulate the pwm frequency to spread out the switching noise?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 01:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Spread-Spectrum-PWM/m-p/758631#M479</guid>
      <dc:creator>geoffreylansber</dc:creator>
      <dc:date>2018-01-03T01:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: Spread Spectrum PWM</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Spread-Spectrum-PWM/m-p/758632#M480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Geoffrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS doesn't feature spread spectrum PWM by default.&amp;nbsp; You should be able to add support for this into KMS.&amp;nbsp; You would do this by replacing the SVPWM block with a new block of your own design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS sets up the PWMs to be center-aligned so that the ADC sample is taken in the middle of the PWM period.&amp;nbsp; So the ADC sample would occur in the same place regardless if the frequency is changing.&amp;nbsp;&amp;nbsp;In addition to modifying the frequency, you would also need to change the deadtime counter since the FlexTimer handles the deadtime insertion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think varying the PWM frequency by a few kHz would impact the control loops within KMS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 14:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Spread-Spectrum-PWM/m-p/758632#M480</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2018-01-03T14:04:00Z</dc:date>
    </item>
  </channel>
</rss>