<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BLDC control project based on AN4862 in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/BLDC-control-project-based-on-AN4862/m-p/732282#M383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm now doing a BLDC control project based on AN4862 . I have modified the EVB for my appliction, so i have some questions about softrware.&lt;/P&gt;&lt;P&gt;i want to define the current AMP gain by myself , how can i modify the code, in which source code file can i find the definition ? Is there a function or formula to calculate actual current .&lt;/P&gt;&lt;P&gt;i want to define the divider resistor of BEMF by myself , how can i modify the code, in which source code file can i find the definition ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The motor can running , but the sound and the temperature are not normall (SlowControlloop) , what parameters can lead this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to haear from you .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Oct 2017 11:32:05 GMT</pubDate>
    <dc:creator>fazhichen</dc:creator>
    <dc:date>2017-10-30T11:32:05Z</dc:date>
    <item>
      <title>BLDC control project based on AN4862</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/BLDC-control-project-based-on-AN4862/m-p/732282#M383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm now doing a BLDC control project based on AN4862 . I have modified the EVB for my appliction, so i have some questions about softrware.&lt;/P&gt;&lt;P&gt;i want to define the current AMP gain by myself , how can i modify the code, in which source code file can i find the definition ? Is there a function or formula to calculate actual current .&lt;/P&gt;&lt;P&gt;i want to define the divider resistor of BEMF by myself , how can i modify the code, in which source code file can i find the definition ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The motor can running , but the sound and the temperature are not normall (SlowControlloop) , what parameters can lead this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to haear from you .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 11:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/BLDC-control-project-based-on-AN4862/m-p/732282#M383</guid>
      <dc:creator>fazhichen</dc:creator>
      <dc:date>2017-10-30T11:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: BLDC control project based on AN4862</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/BLDC-control-project-based-on-AN4862/m-p/732283#M384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fazhi Chen, &lt;BR /&gt;Please refer DRM144, and AN4870. I hope that will answer all your question.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Dec 2017 06:18:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/BLDC-control-project-based-on-AN4862/m-p/732283#M384</guid>
      <dc:creator>mohammad_kamil</dc:creator>
      <dc:date>2017-12-26T06:18:55Z</dc:date>
    </item>
  </channel>
</rss>