<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックRe: Problem connecting TWR-KV46F150M with KMS</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727004#M340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correct. If you decide during your development that you can use your own motor control firmware and not KMS then you do not need to buy the KMS enabled MCU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, since the KV1x, KV3x, and KV4x MCUs&amp;nbsp;offer pin compatible packages it is possible to switch between MCUs depending on the dynamic range requirements of you system.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use KMS in your product in the future then you would change your BOM to include the KMS part you need.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2018 15:46:53 GMT</pubDate>
    <dc:creator>philip_drake</dc:creator>
    <dc:date>2018-05-30T15:46:53Z</dc:date>
    <item>
      <title>Problem connecting TWR-KV46F150M with KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727001#M337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wondering if anyone has used&amp;nbsp;TWR-KV46F150M with KMS I am having the following message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" An issue has prevented communication with target MCU: The ping message was not acknowledged. Please check physical connection to MCU, then navigate to Project menu to configure communication port."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 May 2018 13:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727001#M337</guid>
      <dc:creator>abdullahmamun</dc:creator>
      <dc:date>2018-05-28T13:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting TWR-KV46F150M with KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727002#M338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;TWR-KV46F150M was only recently added to the Kinetis Motor Suite MCUs.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The only boards that have been updated to work with KMS are the boards purchased from NXP.com after&amp;nbsp;January 2018.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The HVP-KV46 purchased before April of 2018 also does not have the KMS library.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;At this point NXP does not have an ordererable KMS part number for the KV46 yet.&amp;nbsp; The goal is to have these available as soon as Q3 of 2018.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Philip&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 May 2018 16:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727002#M338</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2018-05-29T16:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting TWR-KV46F150M with KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727003#M339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philip&lt;/P&gt;&lt;P&gt;Thanks for your reply. Correct me if I am wrong, if I buy a KMS enabled board from NXP.COM and then start the application development with KMS snd mcuxpresso and in the final product if I dont need to use KMS anymore I don't need the KMS enabled chip any more.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Abdullah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 02:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727003#M339</guid>
      <dc:creator>abdullahmamun</dc:creator>
      <dc:date>2018-05-30T02:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problem connecting TWR-KV46F150M with KMS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727004#M340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correct. If you decide during your development that you can use your own motor control firmware and not KMS then you do not need to buy the KMS enabled MCU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, since the KV1x, KV3x, and KV4x MCUs&amp;nbsp;offer pin compatible packages it is possible to switch between MCUs depending on the dynamic range requirements of you system.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use KMS in your product in the future then you would change your BOM to include the KMS part you need.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 15:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Problem-connecting-TWR-KV46F150M-with-KMS/m-p/727004#M340</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2018-05-30T15:46:53Z</dc:date>
    </item>
  </channel>
</rss>