<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error compiling KMS autogenerated code in KDS in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Error-compiling-KMS-autogenerated-code-in-KDS/m-p/712063#M270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the KMS in order to generate C code, but there are still some errors when I try to build it from KDS 3.2. I followed the first example regarding velocity control in Kinetis Motor Suite Lab Guide and I have already installed the necessary software that the tutorial demands.&lt;BR /&gt;Here follows the errors:&lt;BR /&gt;Description Resource Path Location Type&lt;BR /&gt;cannot find -lksdk_platform&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;cannot find -lksdk_startup&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope you could help me!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Aug 2017 21:38:53 GMT</pubDate>
    <dc:creator>PedroCastro</dc:creator>
    <dc:date>2017-08-30T21:38:53Z</dc:date>
    <item>
      <title>Error compiling KMS autogenerated code in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Error-compiling-KMS-autogenerated-code-in-KDS/m-p/712063#M270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the KMS in order to generate C code, but there are still some errors when I try to build it from KDS 3.2. I followed the first example regarding velocity control in Kinetis Motor Suite Lab Guide and I have already installed the necessary software that the tutorial demands.&lt;BR /&gt;Here follows the errors:&lt;BR /&gt;Description Resource Path Location Type&lt;BR /&gt;cannot find -lksdk_platform&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;cannot find -lksdk_startup&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope you could help me!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 21:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Error-compiling-KMS-autogenerated-code-in-KDS/m-p/712063#M270</guid>
      <dc:creator>PedroCastro</dc:creator>
      <dc:date>2017-08-30T21:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error compiling KMS autogenerated code in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Error-compiling-KMS-autogenerated-code-in-KDS/m-p/712064#M271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure you build the platform and startup libraries located in KSDK 1.3. &amp;nbsp;When using KDS you will need to add these projects into your workspace and build them in Release mode. &amp;nbsp;These should be instructions in the lab guide about importing these projects.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 21:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Error-compiling-KMS-autogenerated-code-in-KDS/m-p/712064#M271</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2017-08-31T21:08:09Z</dc:date>
    </item>
  </channel>
</rss>