<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックIncorrect values for rms current and injection current</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693265#M224</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just installed Motor Suite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run it the motor current starts off as 23xxxxxx - some large no. This can be changed to a reasonable current.&amp;nbsp; But then when I try to measure the motor I get this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BrakeParams['DCInjCurrent'] set to 650538254336&lt;/P&gt;&lt;P&gt;Although I can change the alue in protection it is not saved and whenever I try to measure I get a huge number and the same error condition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody come across this before.&amp;nbsp; I have reinstalled a few times.&amp;nbsp; Oh, the motor does run if you bypass the various checks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS_1.1.0 and Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some very helpful person, VB, said that you have to change your region to United States. Something in the Python script goes wrong if your region is South Africa.&amp;nbsp; Quite frankly, I don't know how on earth anybody would find that out!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Aug 2017 12:45:19 GMT</pubDate>
    <dc:creator>gianveglio</dc:creator>
    <dc:date>2017-08-03T12:45:19Z</dc:date>
    <item>
      <title>Incorrect values for rms current and injection current</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693265#M224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just installed Motor Suite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run it the motor current starts off as 23xxxxxx - some large no. This can be changed to a reasonable current.&amp;nbsp; But then when I try to measure the motor I get this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BrakeParams['DCInjCurrent'] set to 650538254336&lt;/P&gt;&lt;P&gt;Although I can change the alue in protection it is not saved and whenever I try to measure I get a huge number and the same error condition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody come across this before.&amp;nbsp; I have reinstalled a few times.&amp;nbsp; Oh, the motor does run if you bypass the various checks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS_1.1.0 and Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some very helpful person, VB, said that you have to change your region to United States. Something in the Python script goes wrong if your region is South Africa.&amp;nbsp; Quite frankly, I don't know how on earth anybody would find that out!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 12:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693265#M224</guid>
      <dc:creator>gianveglio</dc:creator>
      <dc:date>2017-08-03T12:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrect values for rms current and injection current</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693266#M225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Python scripts inside KMS can have issues with certain language settings inside Windows. &amp;nbsp;Obviously we can't test all combinations :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The key is the decimal separator. &amp;nbsp;It should be set to .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change this in the following dialog:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10163i39C797EFFAFAF624/image-size/large?v=v2&amp;amp;px=999" title="2017-08-04 08_27_13-C_C++ - KMS-Release@TWRKV31F120M_SNLESSHALL_KDS_[Targets]_[exe] TWRKV31F120M_SNL.png" alt="2017-08-04 08_27_13-C_C++ - KMS-Release@TWRKV31F120M_SNLESSHALL_KDS_[Targets]_[exe] TWRKV31F120M_SNL.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Control Panel, open "Region and Language", click on "Additional Settings" and change your decimal symbol to .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can send us screenshots of what your existing settings are we can be sure to add that into our testing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 12:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693266#M225</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2017-08-04T12:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrect values for rms current and injection current</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693267#M226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adam&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.  It was quite a relief to get things working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There aren’t many people in South Africa using this so local help is in short supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 15:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Incorrect-values-for-rms-current-and-injection-current/m-p/693267#M226</guid>
      <dc:creator>gianveglio</dc:creator>
      <dc:date>2017-08-04T15:06:24Z</dc:date>
    </item>
  </channel>
</rss>