<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Motor SuiteのトピックMedical documentation</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Medical-documentation/m-p/681715#M200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! We are using KMS for a medical device and we have to do all the documentation about the library.&lt;/P&gt;&lt;P&gt;We have the kinetis motro suite api reference manual. But we need more information about the wrappers functions ( SPEED_RUN, TRAJVEL_RUN).&lt;/P&gt;&lt;P&gt;how does the library work?&lt;/P&gt;&lt;P&gt;does the library have any speed or acceleration limit?&lt;/P&gt;&lt;P&gt;etc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jul 2017 11:48:20 GMT</pubDate>
    <dc:creator>juanmas</dc:creator>
    <dc:date>2017-07-03T11:48:20Z</dc:date>
    <item>
      <title>Medical documentation</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Medical-documentation/m-p/681715#M200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! We are using KMS for a medical device and we have to do all the documentation about the library.&lt;/P&gt;&lt;P&gt;We have the kinetis motro suite api reference manual. But we need more information about the wrappers functions ( SPEED_RUN, TRAJVEL_RUN).&lt;/P&gt;&lt;P&gt;how does the library work?&lt;/P&gt;&lt;P&gt;does the library have any speed or acceleration limit?&lt;/P&gt;&lt;P&gt;etc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 11:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Medical-documentation/m-p/681715#M200</guid>
      <dc:creator>juanmas</dc:creator>
      <dc:date>2017-07-03T11:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: Medical documentation</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Medical-documentation/m-p/681716#M201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Juan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you clarify what additional information you need? &amp;nbsp;The wrapper functions perform the indicated operations. &amp;nbsp;For example SPEED_run calls the speed control loop included with KMS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KMS is based on fixed-point math and is a normalized motor control solution. &amp;nbsp;This means that the maximum possible speed in the system is equal to 1.0 in normalized units. &amp;nbsp;The normalization factor for speed is called FULL_SCALE_SPEED_RPM, it is located in the system.h file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the API reference guide the maximum values for profile limits are provided in the entry for the TRAJVEL_config_t structure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 18:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Medical-documentation/m-p/681716#M201</guid>
      <dc:creator>linestream-adam</dc:creator>
      <dc:date>2017-07-06T18:03:53Z</dc:date>
    </item>
  </channel>
</rss>