<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug interface recommendations for Kinetis and LPC? in Kinetis Motor Suite</title>
    <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Debug-interface-recommendations-for-Kinetis-and-LPC/m-p/2404315#M1000</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265538"&gt;@richard37&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your post!&lt;/P&gt;
&lt;P&gt;You may want to consider a SEGGER J-Link. It supports both Kinetis and LPC devices when used with MCUXpresso, and it is also natively supported by CodeWarrior 11.&lt;/P&gt;
&lt;P&gt;This makes it a good alternative if you need a debug probe that can be used across both development environments and device families.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Aug 2026 17:51:37 GMT</pubDate>
    <dc:creator>carlos_o</dc:creator>
    <dc:date>2026-08-12T17:51:37Z</dc:date>
    <item>
      <title>Debug interface recommendations for Kinetis and LPC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Debug-interface-recommendations-for-Kinetis-and-LPC/m-p/2404221#M999</link>
      <description>&lt;P&gt;I do most of my development on the Kinetis series, and potentially some LPC parts in the near future. I've got a drawer full of debug interfaces from P&amp;amp;E Micro, including a Cyclone ACP that I use most.&lt;/P&gt;&lt;P&gt;I sometimes find myself switching from the $600 Cyclone to the $20 LPC-Link2 because the Cyclone has so many weird problems with MCUXpresso. Honestly the LPC-Link2 does most of what I need, it's just a bit slow.&lt;/P&gt;&lt;P&gt;Should I be looking at Segger interfaces? Can someone recommend a reliable, reasonably fast interface that's well-supported in MCUXpresso (and hopefully CodeWarrior 11 as well) that doesn't cause crashes all of the time, or fail to halt a running target? Trace support would be nice.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 12 Aug 2026 11:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Debug-interface-recommendations-for-Kinetis-and-LPC/m-p/2404221#M999</guid>
      <dc:creator>richard37</dc:creator>
      <dc:date>2026-08-12T11:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: Debug interface recommendations for Kinetis and LPC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Motor-Suite/Debug-interface-recommendations-for-Kinetis-and-LPC/m-p/2404315#M1000</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265538"&gt;@richard37&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your post!&lt;/P&gt;
&lt;P&gt;You may want to consider a SEGGER J-Link. It supports both Kinetis and LPC devices when used with MCUXpresso, and it is also natively supported by CodeWarrior 11.&lt;/P&gt;
&lt;P&gt;This makes it a good alternative if you need a debug probe that can be used across both development environments and device families.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Aug 2026 17:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Motor-Suite/Debug-interface-recommendations-for-Kinetis-and-LPC/m-p/2404315#M1000</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-08-12T17:51:37Z</dc:date>
    </item>
  </channel>
</rss>