<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: Processor Expert High Level Component Missing</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329627#M87</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kashyap,&lt;/P&gt;&lt;P&gt;For which microcontroller did you create the project?&lt;/P&gt;&lt;P&gt;Have you created the project with the Kinetis SDK enabled? If yes, then the Kinetis SDK does not support these components.&lt;/P&gt;&lt;P&gt;Create the project without the SDK enabled, then you should be able to use this components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Dec 2014 06:37:31 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2014-12-06T06:37:31Z</dc:date>
    <item>
      <title>Processor Expert High Level Component Missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329626#M86</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Being new to Kinetis Design Studio and Processor Expert, I was following a tutorial on &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmcuoneclipse.com%2F2013%2F02%2F10%2Ftutorial-adc-with-the-freedom-board%2F" rel="nofollow" target="_blank"&gt;Tutorial: ADC with the Freedom Board | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Issue is the ADC Component which is mentioned in the post to be imported into the Project, is missing in my KDS IDE. I had installed KDS 1.1 and then KSDK. Can Any one help me what is the solution to get ADC high level component back into the component library.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;Kashyap Gada&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2014 06:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329626#M86</guid>
      <dc:creator>kashyapgada</dc:creator>
      <dc:date>2014-12-06T06:18:15Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert High Level Component Missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329627#M87</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kashyap,&lt;/P&gt;&lt;P&gt;For which microcontroller did you create the project?&lt;/P&gt;&lt;P&gt;Have you created the project with the Kinetis SDK enabled? If yes, then the Kinetis SDK does not support these components.&lt;/P&gt;&lt;P&gt;Create the project without the SDK enabled, then you should be able to use this components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2014 06:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329627#M87</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-12-06T06:37:31Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert High Level Component Missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329628#M88</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erich Styger,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I am using KL25z FRDM Board.&amp;nbsp; I donot know if I had enabled/selected the SDK but yes, I did install it on my KDS IDE. I had installed KDS on two machines, and KSDK on only one and not in other. The one in which KSDK was installed I did not find the ADC High Level component, But in the other machine where i didnot install KSDK the same ADC component was available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why are the components not available with KSDK &amp;gt;? What are the benefits of KSDK then?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2014 09:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329628#M88</guid>
      <dc:creator>kashyapgada</dc:creator>
      <dc:date>2014-12-06T09:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert High Level Component Missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329629#M89</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erich Styger,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I am using KL25z FRDM Board.&amp;nbsp; I donot know if I had enabled/selected the SDK but yes, I did install it on my KDS IDE. I had installed KDS on two machines, and KSDK on only one and not in other. The one in which KSDK was installed I did not find the ADC High Level component, But in the other machine where i didnot install KSDK the same ADC component was available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why are the components not available with KSDK &amp;gt;? What are the benefits of KSDK then?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2014 09:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329629#M89</guid>
      <dc:creator>kashyapgada</dc:creator>
      <dc:date>2014-12-06T09:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert High Level Component Missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329630#M90</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Kashyap,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Mr Erich said, currently SDK does not support KL25&amp;nbsp; family. Pls refer to the &amp;lt;&amp;lt;Kinetis SDK release Notes.pdf&amp;gt;&amp;gt; located at:C:\Freescale\KSDK_1.0.0\doc, the KL25 family is not included in the list of processor which SDK supports.&lt;/P&gt;&lt;P&gt;You can use PE to develop code.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 08:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Processor-Expert-High-Level-Component-Missing/m-p/329630#M90</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2014-12-17T08:50:18Z</dc:date>
    </item>
  </channel>
</rss>