<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376841#M866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;Thanks for the info.&amp;nbsp; Where can I find the dev_hid_mouse_frdmk22f120m_bm project?&amp;nbsp; I'd like to take a look at it to see if there is something different in the way the USB is used.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our application the USB is configured as a host (not OTG).&amp;nbsp; I could see that the bootloader left some of the registers configured for OTG, and this is where problems started happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Derek Valleroy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Mar 2015 14:16:50 GMT</pubDate>
    <dc:creator>derekvalleroy</dc:creator>
    <dc:date>2015-03-17T14:16:50Z</dc:date>
    <item>
      <title>KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376839#M864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an application on the K22 that gets bootloaded by the KSDK 1.1.0 bootloader.&amp;nbsp; The bootloader and the application both use USB.&amp;nbsp; I've found that I need to manually reset all the USB registers after the bootload to get my application's USB to work.&amp;nbsp; Has anyone else come across this?&amp;nbsp; I guess I would have thought that the bootloader (FSL_Kinetis_Bootloader_1_1_0) would do this before jumping to the application.&amp;nbsp; Maybe I'm missing something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2015 13:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376839#M864</guid>
      <dc:creator>derekvalleroy</dc:creator>
      <dc:date>2015-03-11T13:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376840#M865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;I just used the flashloader from the FSL_Kinetis_Bootloader_1_1_0 to program dev_hid_mouse_frdmk22f120m_bm from the KSDK 1.1.0 through the USB interface.&lt;/P&gt;&lt;P&gt;After programming process completed, the demo run well, it needn't to reset all the USB registers before the demo start to execute.&lt;/P&gt;&lt;P&gt;I've attached the Demo Applications User-s Guide for the Kinetis K22 Platforms and you can learn the procedure to program the application by the bootloader, please refer to it for details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 07:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376840#M865</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-03-12T07:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376841#M866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;Thanks for the info.&amp;nbsp; Where can I find the dev_hid_mouse_frdmk22f120m_bm project?&amp;nbsp; I'd like to take a look at it to see if there is something different in the way the USB is used.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our application the USB is configured as a host (not OTG).&amp;nbsp; I could see that the bootloader left some of the registers configured for OTG, and this is where problems started happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Derek Valleroy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2015 14:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376841#M866</guid>
      <dc:creator>derekvalleroy</dc:creator>
      <dc:date>2015-03-17T14:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376842#M867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;The demo dev_hid_mouse_frdmk22f120m_bm from the Kinetis SDK 1.1.0 and you can download the develop kit through the link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK&amp;amp;nodeId=0152101E8C1EF7&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK&amp;amp;nodeId=0152101E8C1EF7&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Software Development Kit for Kinetis MCUs|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2015 02:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376842#M867</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-03-18T02:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376843#M868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp; Are you using the SKDK_1.10/usb/example/device/hid/hid_mouse example?&amp;nbsp; I didn't see a mouse in the KSDK_1.1.0/demos folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Derek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2015 13:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376843#M868</guid>
      <dc:creator>derekvalleroy</dc:creator>
      <dc:date>2015-03-18T13:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK 1.1.0 Bootloader isn't Resetting USB Register Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376844#M869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;Sorry, I should list the path of the demo in the last reply.&lt;/P&gt;&lt;P&gt;And he demo reside in the ~:\Freescale\KSDK_1.1.0\usb\example\device\hid\hid_mouse\sdk\iar\dev_hid_mouse_frdmk22f_bm, please refer to it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 03:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-1-0-Bootloader-isn-t-Resetting-USB-Register-Settings/m-p/376844#M869</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-03-19T03:23:48Z</dc:date>
    </item>
  </channel>
</rss>