<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KDS ,fsl_clock_manager ,code not generated for any &amp;quot;device specific&amp;quot; and &amp;quot;common&amp; in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1412435#M8123</link>
    <description>&lt;P&gt;Hello Vicente.&lt;BR /&gt;In years i neved had the time to learn it properly.I've tried,but i was not able to obtain much from MCUXpresso,so i got back to KDS ,being aware that KDS is considered old,if not obsolete .&lt;BR /&gt;Just an example, using MCUXpresso with a very small processor as MKL03Z8 ,shows that there is not a peripheral configuration tool(it exists in KDS),and the code generated for an almost empty project almost fills the available Flash.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Have a nice weekend&lt;BR /&gt;&lt;BR /&gt;Diego&lt;/P&gt;</description>
    <pubDate>Fri, 11 Feb 2022 12:31:43 GMT</pubDate>
    <dc:creator>diegocolombo</dc:creator>
    <dc:date>2022-02-11T12:31:43Z</dc:date>
    <item>
      <title>KDS ,fsl_clock_manager ,code not generated for any "device specific" and "common" methods</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1377601#M8115</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;please can you check what could be wrong?&lt;BR /&gt;&lt;BR /&gt;i'm using MKV11 with KDS with KSDK 1.3.0&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;the fsl_clock_manager component works and generates code ,for example&lt;BR /&gt;CLOCK_HAL_GetFtmFixFreqClkSrc&amp;nbsp; is present&lt;BR /&gt;&lt;BR /&gt;Instead,the generated code of any method in "device" or "common" folder is missing&lt;BR /&gt;&lt;BR /&gt;in Properties-&amp;gt;ProcessorExpert-&amp;gt;Kinetis SDK Specific Options the Library Modes flags "platform_lib" and "startup_lib" are flagged&lt;BR /&gt;ksdk_statrtup_lib_KV11Z7 is present and compiled in workspace and its "\debug" folder path was added&lt;BR /&gt;in Library&amp;nbsp; search path.&lt;BR /&gt;&lt;BR /&gt;Thanks for your help or time&lt;BR /&gt;Diego&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Path startup libraries.png" style="width: 638px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/163323i095C84036ABC38C1/image-size/large?v=v2&amp;amp;px=999" role="button" title="Path startup libraries.png" alt="Path startup libraries.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Path startup libraries.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 11:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1377601#M8115</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2021-11-26T11:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: KDS ,fsl_clock_manager ,code not generated for any "device specific" and "common&amp;</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1380780#M8116</link>
      <description>&lt;P&gt;Would be possible that you move to MCUXpresso?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;Vicente&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 16:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1380780#M8116</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-12-02T16:58:25Z</dc:date>
    </item>
    <item>
      <title>Re: KDS ,fsl_clock_manager ,code not generated for any "device specific" and "common&amp;</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1412435#M8123</link>
      <description>&lt;P&gt;Hello Vicente.&lt;BR /&gt;In years i neved had the time to learn it properly.I've tried,but i was not able to obtain much from MCUXpresso,so i got back to KDS ,being aware that KDS is considered old,if not obsolete .&lt;BR /&gt;Just an example, using MCUXpresso with a very small processor as MKL03Z8 ,shows that there is not a peripheral configuration tool(it exists in KDS),and the code generated for an almost empty project almost fills the available Flash.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Have a nice weekend&lt;BR /&gt;&lt;BR /&gt;Diego&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 12:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KDS-fsl-clock-manager-code-not-generated-for-any-quot-device/m-p/1412435#M8123</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2022-02-11T12:31:43Z</dc:date>
    </item>
  </channel>
</rss>