<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: CAN issues on S32K146</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/CAN-issues-on-S32K146/m-p/989166#M7997</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1) if the message is successfully&amp;nbsp;transmitted without errors, the MB flag is always set at the end of the frame, once EOF is detected. Also the CODE field is changing its value, commonly from 0xC to 0x8.&lt;BR clear="none" /&gt;So check if there is no error detected during message transmission. See if CODE&amp;nbsp;field was changed. If yes, check if the&amp;nbsp;flag can be involuntary cleared by SW, using bit access to clearing flags.&amp;nbsp;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) this is not specified I think. The message is send after the MB wins internal arbitration and on the first opportunity window on the bus (when module sees bus free). If no errors are detected during transmission then the flag is set on EOF detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Dec 2019 09:08:00 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-12-03T09:08:00Z</dc:date>
    <item>
      <title>CAN issues on S32K146</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/CAN-issues-on-S32K146/m-p/989165#M7996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAN communication development on S32K146 microcontroller and facing below issues.&lt;/P&gt;&lt;P&gt;Could you please help us in resolving these.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) After transmission, not able to see respective buffer bit set in IFLAG1 register indicating successful transmission.&lt;/P&gt;&lt;P&gt;We are able to receive the sent 8byte data in CAN2.0B on receiving node.&lt;/P&gt;&lt;P&gt;How to check successful transmission happened on transmitting node?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;2) Within how much time&amp;nbsp;successful&amp;nbsp;transmission should happen. For what timeout should CPU wait polling the IFLAG1 register for respective buffer bit?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sudeendra A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2019 07:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/CAN-issues-on-S32K146/m-p/989165#M7996</guid>
      <dc:creator>sudeendra_s</dc:creator>
      <dc:date>2019-11-29T07:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: CAN issues on S32K146</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/CAN-issues-on-S32K146/m-p/989166#M7997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1) if the message is successfully&amp;nbsp;transmitted without errors, the MB flag is always set at the end of the frame, once EOF is detected. Also the CODE field is changing its value, commonly from 0xC to 0x8.&lt;BR clear="none" /&gt;So check if there is no error detected during message transmission. See if CODE&amp;nbsp;field was changed. If yes, check if the&amp;nbsp;flag can be involuntary cleared by SW, using bit access to clearing flags.&amp;nbsp;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) this is not specified I think. The message is send after the MB wins internal arbitration and on the first opportunity window on the bus (when module sees bus free). If no errors are detected during transmission then the flag is set on EOF detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 09:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/CAN-issues-on-S32K146/m-p/989166#M7997</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-12-03T09:08:00Z</dc:date>
    </item>
  </channel>
</rss>