<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックProject Generator Output Does Not Build</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Project-Generator-Output-Does-Not-Build/m-p/762662#M7762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to port a project to the MKL17Z256VFT4. As a first step I used the project generator and the output does not build. I used the following settings:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SDK 2.3 with FatFS and USB selected&lt;/LI&gt;&lt;LI&gt;Advanced project generation&lt;/LI&gt;&lt;LI&gt;Standalone selected&lt;/LI&gt;&lt;LI&gt;IAR project&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached the unaltered output of of the project generator using these selections, but a quick description is that the build fails in clock_config because the compiler cannot find definitions for several structures and what appear to be enums. A quick search of the reference documentation for the API does not turn up a definition. In addition, I have searched the included project files for the definitions expecting that there were issues in the compiler or linker configuration that could be resolved if I knew the location of the definitions. I was unable to find any file with the definitions. I'm stumped because it doesn't appear the definition exists anywhere, but this is the baseline project.&amp;nbsp;I'm using IAR version 8.11 to compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2018 21:13:01 GMT</pubDate>
    <dc:creator>donweier</dc:creator>
    <dc:date>2018-04-03T21:13:01Z</dc:date>
    <item>
      <title>Project Generator Output Does Not Build</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Project-Generator-Output-Does-Not-Build/m-p/762662#M7762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to port a project to the MKL17Z256VFT4. As a first step I used the project generator and the output does not build. I used the following settings:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SDK 2.3 with FatFS and USB selected&lt;/LI&gt;&lt;LI&gt;Advanced project generation&lt;/LI&gt;&lt;LI&gt;Standalone selected&lt;/LI&gt;&lt;LI&gt;IAR project&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached the unaltered output of of the project generator using these selections, but a quick description is that the build fails in clock_config because the compiler cannot find definitions for several structures and what appear to be enums. A quick search of the reference documentation for the API does not turn up a definition. In addition, I have searched the included project files for the definitions expecting that there were issues in the compiler or linker configuration that could be resolved if I knew the location of the definitions. I was unable to find any file with the definitions. I'm stumped because it doesn't appear the definition exists anywhere, but this is the baseline project.&amp;nbsp;I'm using IAR version 8.11 to compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 21:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Project-Generator-Output-Does-Not-Build/m-p/762662#M7762</guid>
      <dc:creator>donweier</dc:creator>
      <dc:date>2018-04-03T21:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Project Generator Output Does Not Build</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Project-Generator-Output-Does-Not-Build/m-p/762663#M7763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Don,&lt;/P&gt;&lt;P&gt;I'd recommend to use latest version of MCUXpresso Config Tools (V4.0) and re-generate clock_config.* for your processor.&lt;/P&gt;&lt;P&gt;Alternatively, you can generate these files directly on the web &lt;A href="http://mcuxpresso.nxp.com"&gt;http://mcuxpresso.nxp.com&lt;/A&gt; - from dashboard select Config Tools and then select Clock tool.&lt;/P&gt;&lt;P&gt;Hope this help&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 07:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Project-Generator-Output-Does-Not-Build/m-p/762663#M7763</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2018-04-04T07:04:48Z</dc:date>
    </item>
  </channel>
</rss>