<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KSDK  driver version in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-driver-version/m-p/743411#M7704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear my friends,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have some questions.&lt;/P&gt;&lt;P&gt;I get SDK_2.2_MKL25Z128xxx4&amp;nbsp; from MCUXpresso Config Tools（SDK builder）, and I find&amp;nbsp;&amp;nbsp; there have too manay uart driver(such as: cmsis_driver_examples\uart\interrupt_transfer\ cmsis_usart_interrupt_transfer.c&amp;nbsp; &amp;amp;&amp;nbsp; driver_examples\uart\interrupt_transfer\uart_interrupt_transfer.c) , both of them are different, So my question is :&lt;/P&gt;&lt;P&gt;1. which driver version&amp;nbsp; I should choose, Why there have two difference uart-driver&amp;nbsp; version for UART( I know ,stm32 uart drivers is only one)&lt;/P&gt;&lt;P&gt;2. in file MKL25Z4.h, I find two type: UART_Type &amp;amp; UART0_Type&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;#define UART1 ((UART_Type *)UART1_BASE)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;#define UART0 ((UART0_Type *)UART0_BASE)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; what the difference between the two type,&amp;nbsp; &amp;nbsp; and how to use it.&amp;nbsp; ( UART_Type is used for uart1,uart2 ?&amp;nbsp; &amp;nbsp; UART0_Type is only used for uart0 ?,isn't it ?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Nov 2017 05:17:08 GMT</pubDate>
    <dc:creator>randolphwang</dc:creator>
    <dc:date>2017-11-02T05:17:08Z</dc:date>
    <item>
      <title>KSDK  driver version</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-driver-version/m-p/743411#M7704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear my friends,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have some questions.&lt;/P&gt;&lt;P&gt;I get SDK_2.2_MKL25Z128xxx4&amp;nbsp; from MCUXpresso Config Tools（SDK builder）, and I find&amp;nbsp;&amp;nbsp; there have too manay uart driver(such as: cmsis_driver_examples\uart\interrupt_transfer\ cmsis_usart_interrupt_transfer.c&amp;nbsp; &amp;amp;&amp;nbsp; driver_examples\uart\interrupt_transfer\uart_interrupt_transfer.c) , both of them are different, So my question is :&lt;/P&gt;&lt;P&gt;1. which driver version&amp;nbsp; I should choose, Why there have two difference uart-driver&amp;nbsp; version for UART( I know ,stm32 uart drivers is only one)&lt;/P&gt;&lt;P&gt;2. in file MKL25Z4.h, I find two type: UART_Type &amp;amp; UART0_Type&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;#define UART1 ((UART_Type *)UART1_BASE)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;#define UART0 ((UART0_Type *)UART0_BASE)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; what the difference between the two type,&amp;nbsp; &amp;nbsp; and how to use it.&amp;nbsp; ( UART_Type is used for uart1,uart2 ?&amp;nbsp; &amp;nbsp; UART0_Type is only used for uart0 ?,isn't it ?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 05:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-driver-version/m-p/743411#M7704</guid>
      <dc:creator>randolphwang</dc:creator>
      <dc:date>2017-11-02T05:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK  driver version</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-driver-version/m-p/743412#M7705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; &lt;A _jive_internal="true" data-content-finding="Community" data-userid="307116" data-username="randolphwang" href="https://community.nxp.com/people/randolphwang"&gt;Randolph&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use&amp;nbsp; driver_examples\uart, it is for KSDK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;CMSIS driver is the standard api distributes by ARM for Cortex-M cores&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the reference manual for the difference of UART0 and UART1/2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16601iFC1211490A32E407/image-size/large?v=v2&amp;amp;px=999" title="Kl25z Uart 1.PNG.png" alt="Kl25z Uart 1.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice weekend.&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post is helpful, please click the Correct Answer button or helpful. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 08:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-driver-version/m-p/743412#M7705</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-11-03T08:49:39Z</dc:date>
    </item>
  </channel>
</rss>