<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: How to Save Input with pcm Frame scheme ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733156#M7687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;i'm using the Receiveframesync , Receiver bitclock and the Receiver Data Pin of the TWR-K60F120m Evalboard. These Pins are connected with the ADS1278EVM Board from Ti. On this board is the adc placed. Yes i'm using the Receiverbitclock as SCLK for the adc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2018 13:39:59 GMT</pubDate>
    <dc:creator>philippadolph</dc:creator>
    <dc:date>2018-01-03T13:39:59Z</dc:date>
    <item>
      <title>How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733148#M7679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to save a Input signal ( see picture) and don’t know how to configure my i2s for this scheme . I have a frame of 21 words each word 24 bit . Only the first 8 words must be saved. But the adc need the time of 21 words to transmit data again. If the framesyn takes high state the adc send the data daisy chained on the rising edge of the frame sync. How can I realize the scheme in the picture ? Thx for replie&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2017 11:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733148#M7679</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2017-11-24T11:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733149#M7680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Philipp,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your brief description, I understand that you have a stream which has TDM format. The frame convers 21 slots, only the first 8 slots have valid data, the other 13 slots have invalid data. You want to acquire the 8 valid slot data and send them out via I2S format, is it correct?&lt;/P&gt;&lt;P&gt;For the input data stream, it is okay to use SAI module to acquire all slots data, you can discard the invalid 13 slots data and only save the 8 valid data to buffer, it is easy.&lt;/P&gt;&lt;P&gt;But you have to output the valid data stream via I2S format, the difficult task is synchronization, the (input bit clock frequency)/(output bit clock frequency)=21/8. Fortunately, the SAI module supports the feature, you can use the SAI transmitter/receiver in asychronous mode, in the case, transmitter and receiver use independent bit clock and frame clock, youn can connect the bit clock of receiver to MCLK, you can set the FRACT=7, DIVIDE=20, you can get the transmitter bit clock which is (7/21)*(receiver bit clock frequency).&lt;/P&gt;&lt;P&gt;In conclusion, you can use SAI receiver to acquire the valid data and save them in buffer. You can connect the Bit clock of SAI receiver to MCLK, use MCLK clock to get the bit clock of SAI transmitter, then use the SAI transmitter to transfer the 8 valid slot data.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49707iED44D75F9E78FD2D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 08:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733149#M7680</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-12-01T08:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733150#M7681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much, sorry for the late response&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 14:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733150#M7681</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2017-12-21T14:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733151#M7682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The sai with dma communication works fine now. The adc send data to the µC and the µC saves the data via dma. But i lose data. And i don't know how to fix it. I want to implement a continuous communication with the adc. After&amp;nbsp; framesync is set i receive 8 words (25 bit) and 13 words will be ignored. The FIFO request Triggers the dma: watermark sai set on 2; dma Transaction set on 2 request 1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32076i7D0095C33069A19C/image-size/large?v=v2&amp;amp;px=999" title="Unbenann1t.jpg" alt="Unbenann1t.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;red circles = lost data&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 16:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733151#M7682</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2017-12-21T16:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733152#M7683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;here the data i received&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 16:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733152#M7683</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2017-12-21T16:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733153#M7684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Philipp,&lt;/P&gt;&lt;P&gt;i think the desynchronization leads to the problem, how do you generate the I2S transmitter bit clock? the ratio of the I2S transmitter bit clock frequency and TDM receiver bit clcok frequency is 8:21.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Dec 2017 08:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733153#M7684</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-12-25T08:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733154#M7685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SAI Module works in asynchron mod an generate the receiver bit clock and framesync signal . I don't cancel the communications of the EVM and the adc module&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Dec 2017 12:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733154#M7685</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2017-12-29T12:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733155#M7686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Philipp,&lt;/P&gt;&lt;P&gt;Do you use the receiver bit clock as transmitter bit clock? if it is not the case, how do you generate the bit clock of SAI transmitter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 09:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733155#M7686</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-01-03T09:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733156#M7687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;i'm using the Receiveframesync , Receiver bitclock and the Receiver Data Pin of the TWR-K60F120m Evalboard. These Pins are connected with the ADS1278EVM Board from Ti. On this board is the adc placed. Yes i'm using the Receiverbitclock as SCLK for the adc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 13:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733156#M7687</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2018-01-03T13:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733157#M7688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I only want to receive the adc data. there is not transmit from twrk60f120m to the adc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 14:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733157#M7688</guid>
      <dc:creator>philippadolph</dc:creator>
      <dc:date>2018-01-03T14:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to Save Input with pcm Frame scheme ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733158#M7689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Philipp,&lt;/P&gt;&lt;P&gt;Regaring the losing data, I have not idea. If you use DMA to transfer, how about setting the watermark as 1, DMA will fetch one data for one trigger. Secondly, you can use interrupt mechanism to fetch data.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 03:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-Save-Input-with-pcm-Frame-scheme/m-p/733158#M7689</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-01-04T03:17:13Z</dc:date>
    </item>
  </channel>
</rss>