<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Clock drift in tickless idle mode in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Clock-drift-in-tickless-idle-mode/m-p/708873#M7557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what i understand, please correct me if i am wrong, the lptmr was added to tickless idle &amp;nbsp;to minimize time drift during sleep. But from the following comment i can understand the some drift is still possible:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/* Stop the LPTMR and systick momentarily. The time the LPTMR and systick is stopped for&lt;BR /&gt; is accounted for as best it can be, but using the tickless mode will&lt;BR /&gt; inevitably result in some tiny drift of the time maintained by the&lt;BR /&gt; kernel with respect to calendar time. */&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. What is the drift that i should expect in this case?&lt;/P&gt;&lt;P&gt;2. If i need to use LPTMR for other purposes, and will be using&amp;nbsp;fsl_tickless_systick instead of&amp;nbsp;fsl_tickless_lptmr. What is the drift that i should expect in this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Evgeny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Aug 2017 20:42:21 GMT</pubDate>
    <dc:creator>evgenyerlihman</dc:creator>
    <dc:date>2017-08-28T20:42:21Z</dc:date>
    <item>
      <title>Clock drift in tickless idle mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Clock-drift-in-tickless-idle-mode/m-p/708873#M7557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what i understand, please correct me if i am wrong, the lptmr was added to tickless idle &amp;nbsp;to minimize time drift during sleep. But from the following comment i can understand the some drift is still possible:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/* Stop the LPTMR and systick momentarily. The time the LPTMR and systick is stopped for&lt;BR /&gt; is accounted for as best it can be, but using the tickless mode will&lt;BR /&gt; inevitably result in some tiny drift of the time maintained by the&lt;BR /&gt; kernel with respect to calendar time. */&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. What is the drift that i should expect in this case?&lt;/P&gt;&lt;P&gt;2. If i need to use LPTMR for other purposes, and will be using&amp;nbsp;fsl_tickless_systick instead of&amp;nbsp;fsl_tickless_lptmr. What is the drift that i should expect in this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Evgeny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 20:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Clock-drift-in-tickless-idle-mode/m-p/708873#M7557</guid>
      <dc:creator>evgenyerlihman</dc:creator>
      <dc:date>2017-08-28T20:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: Clock drift in tickless idle mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Clock-drift-in-tickless-idle-mode/m-p/708874#M7558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Evgeny,&lt;/P&gt;&lt;P&gt;regardless what timer you are going to use, you will have some drift. The drift is caused by the fact that in tickless idle mode the timer is not continuously running, but the RTOS has to&lt;/P&gt;&lt;P&gt;a) stop the timer&lt;/P&gt;&lt;P&gt;b) update the timer modulo register with the new value&lt;/P&gt;&lt;P&gt;c) restart the timer&lt;/P&gt;&lt;P&gt;This for every tickless timer interrupt. Now how much the drift will be depends on the timer interrupt frequency.&lt;/P&gt;&lt;P&gt;The LPTMR adds some extra drift because the minimal time for the tick is 1 ms. So in the worst case you will be off up to 1ms for every timer tick. In my applications I have a drift in the range of or 10% using LPTMR, and in the range of 2-5% for high frequency SysTick timer.&lt;/P&gt;&lt;P&gt;Note that you can add a compensation with using configSTOPPED_TIMER_COMPENSATION.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More infos: &lt;A class="link-titled" href="http://www.freertos.org/low-power-tickless-rtos.html" title="http://www.freertos.org/low-power-tickless-rtos.html"&gt;Tickless Low power features in FreeRTOS&lt;/A&gt; and &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/07/06/low-power-with-freertos-tickless-idle-mode/" title="https://mcuoneclipse.com/2013/07/06/low-power-with-freertos-tickless-idle-mode/"&gt;Low Power with FreeRTOS: Tickless Idle Mode | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 06:37:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Clock-drift-in-tickless-idle-mode/m-p/708874#M7558</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-08-29T06:37:17Z</dc:date>
    </item>
  </channel>
</rss>