<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックIs lwIP MISRA Compliant MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Is-lwIP-MISRA-Compliant-MCUXpresso-SDK/m-p/695288#M7471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have gone through the MCU Xpresso SDK manual. It is stated that the start code and drivers are MISRA compliant. I wanted to ask that whether the optional middle ware(lwIP) is MISRA compliant or not. If it is compliant, then is it 2004 or 2012.The board I am using in FRDM-K64F and my application requires a TCP/IP Stack but also requires MISRA Compliance. Any help will be highly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abdullah Shafiq&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Sep 2017 13:27:29 GMT</pubDate>
    <dc:creator>abdullahshafiq</dc:creator>
    <dc:date>2017-09-29T13:27:29Z</dc:date>
    <item>
      <title>Is lwIP MISRA Compliant MCUXpresso SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Is-lwIP-MISRA-Compliant-MCUXpresso-SDK/m-p/695288#M7471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have gone through the MCU Xpresso SDK manual. It is stated that the start code and drivers are MISRA compliant. I wanted to ask that whether the optional middle ware(lwIP) is MISRA compliant or not. If it is compliant, then is it 2004 or 2012.The board I am using in FRDM-K64F and my application requires a TCP/IP Stack but also requires MISRA Compliance. Any help will be highly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abdullah Shafiq&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 13:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Is-lwIP-MISRA-Compliant-MCUXpresso-SDK/m-p/695288#M7471</guid>
      <dc:creator>abdullahshafiq</dc:creator>
      <dc:date>2017-09-29T13:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Is lwIP MISRA Compliant MCUXpresso SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Is-lwIP-MISRA-Compliant-MCUXpresso-SDK/m-p/695289#M7472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="303630" data-username="abdullahshafiq" href="https://community.nxp.com/people/abdullahshafiq"&gt;Abdullah Shafiq&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No,&amp;nbsp; only&amp;nbsp; code we developed as a part of MCUSDK – drivers and USB stack are MISRA compliant. &amp;nbsp;3&lt;SUP&gt;rd&lt;/SUP&gt; party code such as LWIP is not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2017 14:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Is-lwIP-MISRA-Compliant-MCUXpresso-SDK/m-p/695289#M7472</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-10-05T14:24:21Z</dc:date>
    </item>
  </channel>
</rss>