<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックIssue with CAN(TX) using KEAZ128 and SDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Issue-with-CAN-TX-using-KEAZ128-and-SDK/m-p/684876#M7420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using one of the examples i found on this community. I am using FRDM- KEAZ128 development board and want to send CAN data from the board( TX). Moreover i am using SDK instead of using code warrior.( i believe i took this code from one of the posts that mentions the problem with using NVIC.h file for SDK platform, and then someone uploaded a code compatible with SDK) I can compile the code without any issues, however, when i put it in debug mode, i can see a path error. I tried updating the path from source lookup path preferences, but i am still getting a path issue which throws an error : No source available for init CAN() at 0 x 498.&lt;/P&gt;&lt;P&gt;I am new to this platform and not sure where i am going wrong. The code is attached with this post.&lt;/P&gt;&lt;P&gt;Can someone please help me understanding the issue.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339191"&gt;KEAZ128_Community_MSCAN.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 12:57:55 GMT</pubDate>
    <dc:creator>aveshshah</dc:creator>
    <dc:date>2017-06-13T12:57:55Z</dc:date>
    <item>
      <title>Issue with CAN(TX) using KEAZ128 and SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Issue-with-CAN-TX-using-KEAZ128-and-SDK/m-p/684876#M7420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using one of the examples i found on this community. I am using FRDM- KEAZ128 development board and want to send CAN data from the board( TX). Moreover i am using SDK instead of using code warrior.( i believe i took this code from one of the posts that mentions the problem with using NVIC.h file for SDK platform, and then someone uploaded a code compatible with SDK) I can compile the code without any issues, however, when i put it in debug mode, i can see a path error. I tried updating the path from source lookup path preferences, but i am still getting a path issue which throws an error : No source available for init CAN() at 0 x 498.&lt;/P&gt;&lt;P&gt;I am new to this platform and not sure where i am going wrong. The code is attached with this post.&lt;/P&gt;&lt;P&gt;Can someone please help me understanding the issue.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339191"&gt;KEAZ128_Community_MSCAN.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 12:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Issue-with-CAN-TX-using-KEAZ128-and-SDK/m-p/684876#M7420</guid>
      <dc:creator>aveshshah</dc:creator>
      <dc:date>2017-06-13T12:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with CAN(TX) using KEAZ128 and SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Issue-with-CAN-TX-using-KEAZ128-and-SDK/m-p/684877#M7421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Avesh Shah,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FRDM-KEA128 MSCAN need to control the on board SBC chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can refer to this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/453806"&gt;FRDM-KEAZ128Q80 MSCAN Communication&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Floor 2, one of the customer already share the according project which is based on the S32DS IDE.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The S32DS IDE can be download in this link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/s32-processors-microcontrollers/s32-design-studio-ide:S32DS?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/s32-processors-microcontrollers/s32-design-studio-ide:S32DS?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;S32 Design Studio IDE|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try it at first.&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 06:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Issue-with-CAN-TX-using-KEAZ128-and-SDK/m-p/684877#M7421</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-07-11T06:34:20Z</dc:date>
    </item>
  </channel>
</rss>