<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックKSDK_1.3.0 DSPI issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-3-0-DSPI-issue/m-p/658290#M7142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, im using SPI and the fsl_dspi official driver, I noticed that when I used &lt;STRONG&gt;DSPI_MasterTransferBlocking&lt;/STRONG&gt; function, i got an unhandled interrupt .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my setup: KSDK_1.3.0 board: frdmk64f.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 08:18:14 GMT</pubDate>
    <dc:creator>carlossilva</dc:creator>
    <dc:date>2017-02-22T08:18:14Z</dc:date>
    <item>
      <title>KSDK_1.3.0 DSPI issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-3-0-DSPI-issue/m-p/658290#M7142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, im using SPI and the fsl_dspi official driver, I noticed that when I used &lt;STRONG&gt;DSPI_MasterTransferBlocking&lt;/STRONG&gt; function, i got an unhandled interrupt .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my setup: KSDK_1.3.0 board: frdmk64f.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 08:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-3-0-DSPI-issue/m-p/658290#M7142</guid>
      <dc:creator>carlossilva</dc:creator>
      <dc:date>2017-02-22T08:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK_1.3.0 DSPI issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-3-0-DSPI-issue/m-p/658291#M7143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the unhandled interrupt occurs, pls check the interrupt source index in the xpsr in debugger of the tools you are using, the bit0~8 of xpsr register represent the interrupt source index.&lt;/P&gt;&lt;P&gt;If the interrupt source index is 3(hard fault interrupt), it is a bit complicated, for example you use a peripheral whose clock is not enabled, or you access a memory which does not exist, all of the case can lead to hardware fault interrupt.&lt;/P&gt;&lt;P&gt;Anyway, i suggest you download SDK2.0 package from the link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/ksdk"&gt;http://www.nxp.com/ksdk&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 07:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-1-3-0-DSPI-issue/m-p/658291#M7143</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-02-27T07:17:45Z</dc:date>
    </item>
  </channel>
</rss>