<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL26Z SPI0 FIFO in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643658#M6921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for that information.&lt;/P&gt;&lt;P&gt;*&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;shaking head&lt;/SPAN&gt;&lt;/SPAN&gt;*&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2016 09:26:28 GMT</pubDate>
    <dc:creator>nobodyKnows</dc:creator>
    <dc:date>2016-09-23T09:26:28Z</dc:date>
    <item>
      <title>KL26Z SPI0 FIFO</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643656#M6919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;it seem that the SPI0 of the KL26Z has no FIFO. I get an Hardfault error if I try to write the SPI0-&amp;gt;C3 register. But according to Page 681 in Reference Manual there is a SPI0_C3 register.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 14:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643656#M6919</guid>
      <dc:creator>nobodyKnows</dc:creator>
      <dc:date>2016-09-22T14:03:58Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z SPI0 FIFO</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643657#M6920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;Pls refer to section 3.9.2 SPI configuration, only SPI1 has 4-deep FIFO of 16 bits entries, the SPI0 module does not have FIFO.&lt;/P&gt;&lt;P&gt;hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I copy it here:&lt;/P&gt;&lt;P&gt;3.9.2.1 SPI instantiation information&lt;BR /&gt;The number of SPI modules on this device is: two&lt;BR /&gt;The supported data length is: 16-bit&lt;BR /&gt;SPI1 includes a 4-deep FIFO of 16-bit entries.&lt;BR /&gt;SPI0 is clocked on the bus clock. That is, the SPI0 module clock is connected to the chiplevel&lt;BR /&gt;bus clock.&lt;BR /&gt;SPI1 is clocked from the system clock. That is, the SPI1 module clock is connected to the&lt;BR /&gt;chip-level system clock. SPI1 is therefore disabled in Partial Stop Mode.&lt;BR /&gt;The SPI supports DMA request and can operate in VLPS mode. When the SPI is&lt;BR /&gt;operating in VLPS mode, it will operate as a slave.&lt;BR /&gt;SPI can wake the MCU from VLPS mode upon reception of SPI data in slave mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 09:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643657#M6920</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-23T09:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: KL26Z SPI0 FIFO</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643658#M6921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for that information.&lt;/P&gt;&lt;P&gt;*&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;shaking head&lt;/SPAN&gt;&lt;/SPAN&gt;*&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 09:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KL26Z-SPI0-FIFO/m-p/643658#M6921</guid>
      <dc:creator>nobodyKnows</dc:creator>
      <dc:date>2016-09-23T09:26:28Z</dc:date>
    </item>
  </channel>
</rss>