<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: MK10DX256VLH7 Support in KSDK 2.0</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642256#M6912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iva,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the quick response. I already have a project in KSDK 2.0 with MK22 and i was hoping to reuse a significant chunk that interfaces with a module for the MK10DX256VLH7 based project. i was hoping to create a project with MK10DX256XXX10 as the base with KSDK2.0 and just use that. Will that not work? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 13:10:43 GMT</pubDate>
    <dc:creator>santosh1</dc:creator>
    <dc:date>2016-09-22T13:10:43Z</dc:date>
    <item>
      <title>MK10DX256VLH7 Support in KSDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642254#M6910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The SDK builder hosted at kex.nxp.com doesn't seem to be supporting MK10DX256VLH7. Uploading a new configuration with processor changed also does not help. Is there any way to download the full SDK or is this controller not supported at all?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 11:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642254#M6910</guid>
      <dc:creator>santosh1</dc:creator>
      <dc:date>2016-09-22T11:10:58Z</dc:date>
    </item>
    <item>
      <title>Re: MK10DX256VLH7 Support in KSDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642255#M6911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Santosh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there is no KSDK support for MK10DX256VLH7.&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Anyway, you can start your program with PEx and KDS.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5520i3C1B20A1C8061F7B/image-size/large?v=v2&amp;amp;px=999" title="MK10.png" alt="MK10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you can start with &lt;A href="http://www.nxp.com/mqx"&gt;www.nxp.com/mqx &lt;/A&gt;also see the support for TWR-K20D72M&lt;/P&gt;&lt;P&gt;For MQX 4.2 is under&lt;/P&gt;&lt;P&gt;&lt;EM&gt;C:\Freescale\Freescale_MQX_4_2\mqx\examples&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 13:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642255#M6911</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2016-09-22T13:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: MK10DX256VLH7 Support in KSDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642256#M6912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iva,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the quick response. I already have a project in KSDK 2.0 with MK22 and i was hoping to reuse a significant chunk that interfaces with a module for the MK10DX256VLH7 based project. i was hoping to create a project with MK10DX256XXX10 as the base with KSDK2.0 and just use that. Will that not work? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 13:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/MK10DX256VLH7-Support-in-KSDK-2-0/m-p/642256#M6912</guid>
      <dc:creator>santosh1</dc:creator>
      <dc:date>2016-09-22T13:10:43Z</dc:date>
    </item>
  </channel>
</rss>