<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: kl25: the watchdog example &amp;quot;cop&amp;quot; doesn't reset cpu in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/kl25-the-watchdog-example-quot-cop-quot-doesn-t-reset-cpu/m-p/634774#M6809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What platform are you running (IAR/GCC/ARM)?&lt;BR /&gt;&lt;BR /&gt;In some of the start up files the COP disabled early on so that it does not fire while the startup code runs.&lt;BR /&gt;As the COP control register is a Write-Once-After-Reset that means the COP can not be used unless the startup code that disables it is found and changed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Apr 2017 13:07:24 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2017-04-03T13:07:24Z</dc:date>
    <item>
      <title>kl25: the watchdog example "cop" doesn't reset cpu</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/kl25-the-watchdog-example-quot-cop-quot-doesn-t-reset-cpu/m-p/634773#M6808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this "cop" example supposed to work with emulator connected?&lt;/P&gt;&lt;P&gt;The code doesn't reset cpu.&lt;/P&gt;&lt;P&gt;I also tried writing wrong value to SRVCOP (SIM-&amp;gt;SRVCOP = 0; ) which should cause reset but it doesn't.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 12:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/kl25-the-watchdog-example-quot-cop-quot-doesn-t-reset-cpu/m-p/634773#M6808</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-03-30T12:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: kl25: the watchdog example "cop" doesn't reset cpu</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/kl25-the-watchdog-example-quot-cop-quot-doesn-t-reset-cpu/m-p/634774#M6809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What platform are you running (IAR/GCC/ARM)?&lt;BR /&gt;&lt;BR /&gt;In some of the start up files the COP disabled early on so that it does not fire while the startup code runs.&lt;BR /&gt;As the COP control register is a Write-Once-After-Reset that means the COP can not be used unless the startup code that disables it is found and changed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 13:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/kl25-the-watchdog-example-quot-cop-quot-doesn-t-reset-cpu/m-p/634774#M6809</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2017-04-03T13:07:24Z</dc:date>
    </item>
  </channel>
</rss>