<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: Typo on Kinetis SDK v.2.1 API Reference Manual, for UART Send/receive using an interrupt method</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Typo-on-Kinetis-SDK-v-2-1-API-Reference-Manual-for-UART-Send/m-p/632799#M6769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ChaoXi,&lt;/P&gt;&lt;P&gt;Thank you for pointing out the typo, I will notify the DOC team of modifying it.&lt;/P&gt;&lt;P&gt;The correct prototype of the function is:&lt;/P&gt;&lt;P&gt;status_t UART_TransferSendNonBlocking (UART_Type&amp;nbsp; base, uart_handle_t&amp;nbsp; handle, uart_-&lt;BR /&gt;transfer_t&amp;nbsp; xfer)&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 01:47:52 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-01-24T01:47:52Z</dc:date>
    <item>
      <title>Typo on Kinetis SDK v.2.1 API Reference Manual, for UART Send/receive using an interrupt method</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Typo-on-Kinetis-SDK-v-2-1-API-Reference-Manual-for-UART-Send/m-p/632798#M6768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I read "Kinetis SDK v.2.1 API Reference Manual", as the read box in below, is should be "UART1"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122772i9A431DB0DD70430A/image-size/large?v=v2&amp;amp;px=999" title="174843_174843.png" alt="174843_174843.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12268iDC4B5DF31F40155B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Cai.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 02:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Typo-on-Kinetis-SDK-v-2-1-API-Reference-Manual-for-UART-Send/m-p/632798#M6768</guid>
      <dc:creator>phantomgz</dc:creator>
      <dc:date>2017-01-20T02:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: Typo on Kinetis SDK v.2.1 API Reference Manual, for UART Send/receive using an interrupt method</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Typo-on-Kinetis-SDK-v-2-1-API-Reference-Manual-for-UART-Send/m-p/632799#M6769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ChaoXi,&lt;/P&gt;&lt;P&gt;Thank you for pointing out the typo, I will notify the DOC team of modifying it.&lt;/P&gt;&lt;P&gt;The correct prototype of the function is:&lt;/P&gt;&lt;P&gt;status_t UART_TransferSendNonBlocking (UART_Type&amp;nbsp; base, uart_handle_t&amp;nbsp; handle, uart_-&lt;BR /&gt;transfer_t&amp;nbsp; xfer)&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 01:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Typo-on-Kinetis-SDK-v-2-1-API-Reference-Manual-for-UART-Send/m-p/632799#M6769</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-01-24T01:47:52Z</dc:date>
    </item>
  </channel>
</rss>