<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Has SDK 2.0 been tested on LS1043ARDB in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Has-SDK-2-0-been-tested-on-LS1043ARDB/m-p/628992#M6670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="209722" data-username="stacym" href="https://community.nxp.com/people/stacym"&gt;stacym&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK 2.0 has already been tested on LS1043ARDB, please download the pre_built image ISO QorIQ-SDK-V2.0-AARCH64-IMAGE-20160527-yocto.iso from &lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab" title="http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab"&gt;Linux® SDK for QorIQ ® Processors|NXP&lt;/A&gt; , and try to use these images on LS1043ARDB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also update u-boot image to bank 4 at bank 0 as the following,&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp 82000000 &amp;lt;u-boot_file_name&amp;gt;.bin&lt;BR /&gt;=&amp;gt;protect off 64100000 +$filesize&lt;BR /&gt;=&amp;gt;erase 64100000 +$filesize&lt;BR /&gt;=&amp;gt;cp.b 82000000 64100000 $filesize&lt;BR /&gt;=&amp;gt;protect on 64100000 +$filesize&lt;BR /&gt;=&amp;gt;cpld reset altbank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, please use FIT image(kernel.itb) directly, which includes Linux Kernel, dts and rootfs filesystem.&lt;/P&gt;&lt;P&gt;Please refer to the following procedure.&lt;/P&gt;&lt;P&gt;=&amp;gt;setenv bootargs ‘root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 console=ttyS0,115200’&lt;BR /&gt;=&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp a0000000 &amp;lt; FIT_image_name&amp;gt;&lt;BR /&gt;=&amp;gt;bootm a0000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, would you please provide the whole u-boot and Linux Kernel booting up log?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Apr 2017 08:40:46 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2017-04-11T08:40:46Z</dc:date>
    <item>
      <title>Has SDK 2.0 been tested on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Has-SDK-2-0-been-tested-on-LS1043ARDB/m-p/628991#M6669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having difficulty getting the build of SDK 2.0 to boot on the LS1043ARDB, it freezes/hangs at Starting kernel...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had SDK 0.5 and Kernel 3.19 working on the same board and even tried using the DTB file from that with the new SDK. &amp;nbsp;That gets quite a bit further, it boots to a login prompt but the Ethernet &amp;nbsp;port does not come up. &amp;nbsp;Looking back at the boot messages, the following problems occur during boot:&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.502038] fsl-fman 1a00000.fman: ReadFmDevTreeNode: Failed to get FM clock structure&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.509955] fsl-fman: probe of 1a00000.fman failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.516022] Freescale FM module, FMD API version 21.1.0&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.521292] fsl-fman-port: probe of 1a82000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.527732] fsl-fman-port: probe of 1a83000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.534179] fsl-fman-port: probe of 1a84000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.540624] fsl-fman-port: probe of 1a85000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.547064] fsl-fman-port: probe of 1a86000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.553509] fsl-fman-port: probe of 1a87000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.559968] fsl-fman-port: probe of 1a88000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.566409] fsl-fman-port: probe of 1aa8000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.572858] fsl-fman-port: probe of 1a89000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.579304] fsl-fman-port: probe of 1aa9000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.585747] fsl-fman-port: probe of 1a8a000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.592192] fsl-fman-port: probe of 1aaa000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.598641] fsl-fman-port: probe of 1a8b000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.605081] fsl-fman-port: probe of 1aab000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.611530] fsl-fman-port: probe of 1a8c000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.617970] fsl-fman-port: probe of 1aac000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.624418] fsl-fman-port: probe of 1a8d000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.630864] fsl-fman-port: probe of 1aad000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.637307] fsl-fman-port: probe of 1a90000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.643753] fsl-fman-port: probe of 1ab0000.port failed with error -5&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.650284] Freescale FM Ports module&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.653936] fsl_mac: fsl_mac: FSL FMan MAC API based driver&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.659559] fsl_mac 1ae0000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.665833] fsl_mac 1ae2000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.672110] fsl_mac 1ae4000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.678382] fsl_mac 1ae6000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.684659] fsl_mac 1ae8000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.690935] fsl_mac 1aea000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.697207] fsl_mac 1af0000.ethernet: fm_bind(/fman@1a00000) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.703542] fsl_dpa: FSL DPAA Ethernet driver&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.708009] fsl_dpa fsl,dpaa:ethernet@0: dev_get_drvdata(1ae0000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.715493] fsl_dpa: probe of fsl,dpaa:ethernet@0 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.722125] fsl_dpa fsl,dpaa:ethernet@1: dev_get_drvdata(1ae2000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.729605] fsl_dpa: probe of fsl,dpaa:ethernet@1 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.736231] fsl_dpa fsl,dpaa:ethernet@2: dev_get_drvdata(1ae4000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.743711] fsl_dpa: probe of fsl,dpaa:ethernet@2 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.750343] fsl_dpa fsl,dpaa:ethernet@3: dev_get_drvdata(1ae6000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.757817] fsl_dpa: probe of fsl,dpaa:ethernet@3 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.764450] fsl_dpa fsl,dpaa:ethernet@4: dev_get_drvdata(1ae8000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.771930] fsl_dpa: probe of fsl,dpaa:ethernet@4 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.778558] fsl_dpa fsl,dpaa:ethernet@5: dev_get_drvdata(1aea000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.786037] fsl_dpa: probe of fsl,dpaa:ethernet@5 failed with error -22&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.792670] fsl_dpa fsl,dpaa:ethernet@8: dev_get_drvdata(1af0000.ethernet) failed&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.800150] fsl_dpa: probe of fsl,dpaa:ethernet@8 failed with error -22&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;date: invalid date '0310014735201703'&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...&lt;/P&gt;&lt;P&gt;Running postinst /etc/rpm-postinsts/101-inetutils-inetd...&lt;/P&gt;&lt;P&gt;Running postinst /etc/rpm-postinsts/102-inetutils-ftpd...&lt;/P&gt;&lt;P&gt;INIT: Entering runlevel: 5un-postinsts exists during rc.d purge&lt;/P&gt;&lt;P&gt;Configuring network interfaces... ifup: can't open '/etc/network/interfaces': No such file or directory&lt;/P&gt;&lt;P&gt;Starting OpenBSD Secure Shell server: sshd&lt;/P&gt;&lt;P&gt;&amp;nbsp; generating ssh RSA key...&lt;/P&gt;&lt;P&gt;&amp;nbsp; generating ssh ECDSA key...&lt;/P&gt;&lt;P&gt;&amp;nbsp; generating ssh DSA key...&lt;/P&gt;&lt;P&gt;&amp;nbsp; generating ssh ED25519 key...&lt;/P&gt;&lt;P&gt;Privilege separation user sshd does not exist&lt;/P&gt;&lt;P&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;/P&gt;&lt;P&gt;Starting network benchmark server: netserver.&lt;/P&gt;&lt;P&gt;Starting system log daemon...0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering if the 2.0 SDK was tested on the board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Stacy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 19:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Has-SDK-2-0-been-tested-on-LS1043ARDB/m-p/628991#M6669</guid>
      <dc:creator>stacym</dc:creator>
      <dc:date>2017-03-28T19:46:16Z</dc:date>
    </item>
    <item>
      <title>Re: Has SDK 2.0 been tested on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Has-SDK-2-0-been-tested-on-LS1043ARDB/m-p/628992#M6670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="209722" data-username="stacym" href="https://community.nxp.com/people/stacym"&gt;stacym&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK 2.0 has already been tested on LS1043ARDB, please download the pre_built image ISO QorIQ-SDK-V2.0-AARCH64-IMAGE-20160527-yocto.iso from &lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab" title="http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab"&gt;Linux® SDK for QorIQ ® Processors|NXP&lt;/A&gt; , and try to use these images on LS1043ARDB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also update u-boot image to bank 4 at bank 0 as the following,&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp 82000000 &amp;lt;u-boot_file_name&amp;gt;.bin&lt;BR /&gt;=&amp;gt;protect off 64100000 +$filesize&lt;BR /&gt;=&amp;gt;erase 64100000 +$filesize&lt;BR /&gt;=&amp;gt;cp.b 82000000 64100000 $filesize&lt;BR /&gt;=&amp;gt;protect on 64100000 +$filesize&lt;BR /&gt;=&amp;gt;cpld reset altbank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, please use FIT image(kernel.itb) directly, which includes Linux Kernel, dts and rootfs filesystem.&lt;/P&gt;&lt;P&gt;Please refer to the following procedure.&lt;/P&gt;&lt;P&gt;=&amp;gt;setenv bootargs ‘root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 console=ttyS0,115200’&lt;BR /&gt;=&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp a0000000 &amp;lt; FIT_image_name&amp;gt;&lt;BR /&gt;=&amp;gt;bootm a0000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, would you please provide the whole u-boot and Linux Kernel booting up log?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2017 08:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Has-SDK-2-0-been-tested-on-LS1043ARDB/m-p/628992#M6670</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-04-11T08:40:46Z</dc:date>
    </item>
  </channel>
</rss>