<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: KSDK Power manager</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363810#M654</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alright, thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will fully test this during the system integration phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2015 14:51:06 GMT</pubDate>
    <dc:creator>andersbergström</dc:creator>
    <dc:date>2015-02-03T14:51:06Z</dc:date>
    <item>
      <title>KSDK Power manager</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363808#M652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are currently using KSDK 1.0 with KDS 1.1.1. The application uses FreeRTOS.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To set the application into mode with power manager, mode&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;: kPowerManagerVlps is no problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, we want to wake up the application, either via CAN or Ethernet.&lt;/P&gt;&lt;P&gt;When reading the reference manual for the K&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;64, the wake-up method seems&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;to be interrupt. Do we need to set the system back into mode: kPowerManagerRun and where do we&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;place the function call for that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2015 09:59:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363808#M652</guid>
      <dc:creator>andersbergström</dc:creator>
      <dc:date>2015-01-21T09:59:22Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK Power manager</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363809#M653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anders,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems CAN can wake the system up from VLPS mode, so it should be no problem to use CAN module as the wakeup source under VLPS mode, please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49488iB80FA749614E80DC/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 03:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363809#M653</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2015-01-23T03:10:11Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK Power manager</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363810#M654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alright, thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will fully test this during the system integration phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 14:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-Power-manager/m-p/363810#M654</guid>
      <dc:creator>andersbergström</dc:creator>
      <dc:date>2015-02-03T14:51:06Z</dc:date>
    </item>
  </channel>
</rss>