<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: SPI Master and Slave</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Master-and-Slave/m-p/623161#M6531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kian Seng Koh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain more your settings, it is complicate to follow what the problem could be.&lt;/P&gt;&lt;P&gt;For Processor Expert projects we recommend to check the propierities&amp;nbsp; of the component that is been used, you can right click in the component and go to "help on component". You can also check the examples of KSDK 1.3 for the dspi driver and see if you can run the code without problems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Mar 2017 01:20:39 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-03-09T01:20:39Z</dc:date>
    <item>
      <title>SPI Master and Slave</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Master-and-Slave/m-p/623160#M6530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using two MK64FN and KDS 3.2 with KSDK 1.3. I want to implement SPI master and slave. I use ProcessExpert to add component 'DPSI' and configure Master and Slave configurations. The slave no reply (using DSPI_DRV_SlaveTransferBlocking (as I can see the Master signal on scope)&amp;nbsp;and also the Events.c (SPI_1_IRQHandler) seems not working.&amp;nbsp;Connection: SPI0-SPI1, SIN-SOUT, SOUT-SIN, CLK-CLK-, CS-CS.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 04:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Master-and-Slave/m-p/623160#M6530</guid>
      <dc:creator>kiansengkoh</dc:creator>
      <dc:date>2017-03-06T04:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Master and Slave</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Master-and-Slave/m-p/623161#M6531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kian Seng Koh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain more your settings, it is complicate to follow what the problem could be.&lt;/P&gt;&lt;P&gt;For Processor Expert projects we recommend to check the propierities&amp;nbsp; of the component that is been used, you can right click in the component and go to "help on component". You can also check the examples of KSDK 1.3 for the dspi driver and see if you can run the code without problems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 01:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Master-and-Slave/m-p/623161#M6531</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-03-09T01:20:39Z</dc:date>
    </item>
  </channel>
</rss>