<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic External oscillator cannot start in MKL81 in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/External-oscillator-cannot-start-in-MKL81/m-p/622598#M6498</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem to start external oscillator. The problem is pin XTAL0 goes to high but toggling, so EXTAL0 always stays low.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The hardware design is followed Freedom-KL82 reference design. The external Osc is a 12MHz one. I am using SDK's GPIO example IAR project for&amp;nbsp;frdmkl81z board. In BOARD_ClockInit() function, XTAL0 and EXTAL0 are both configured to alternate 0 mode. I am using default clock configure RUN table which enables OSCERCLK.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I run the code, code stuck in this line, "while(!CLOCK_HAL_IsOsc0Stable(base)){}“. When I put a probe on Oscillator pin 1, I can see PIN XTAL0 stays in HIGH instead of toggling. I think this may cause external Oscillator no output to microprocessor.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone had this problem before?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 01:28:48 GMT</pubDate>
    <dc:creator>daweiy</dc:creator>
    <dc:date>2017-01-17T01:28:48Z</dc:date>
    <item>
      <title>External oscillator cannot start in MKL81</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/External-oscillator-cannot-start-in-MKL81/m-p/622598#M6498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a problem to start external oscillator. The problem is pin XTAL0 goes to high but toggling, so EXTAL0 always stays low.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The hardware design is followed Freedom-KL82 reference design. The external Osc is a 12MHz one. I am using SDK's GPIO example IAR project for&amp;nbsp;frdmkl81z board. In BOARD_ClockInit() function, XTAL0 and EXTAL0 are both configured to alternate 0 mode. I am using default clock configure RUN table which enables OSCERCLK.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I run the code, code stuck in this line, "while(!CLOCK_HAL_IsOsc0Stable(base)){}“. When I put a probe on Oscillator pin 1, I can see PIN XTAL0 stays in HIGH instead of toggling. I think this may cause external Oscillator no output to microprocessor.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone had this problem before?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 01:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/External-oscillator-cannot-start-in-MKL81/m-p/622598#M6498</guid>
      <dc:creator>daweiy</dc:creator>
      <dc:date>2017-01-17T01:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: External oscillator cannot start in MKL81</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/External-oscillator-cannot-start-in-MKL81/m-p/622599#M6499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found out the problem. One of the capacitor shorted to ground which causes EXTAL0 pin stays low all the time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 00:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/External-oscillator-cannot-start-in-MKL81/m-p/622599#M6499</guid>
      <dc:creator>daweiy</dc:creator>
      <dc:date>2017-01-19T00:41:32Z</dc:date>
    </item>
  </channel>
</rss>