<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Kinetis SDK USB abort</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Kinetis-SDK-USB-abort/m-p/612266#M6343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on MK22F I run USB CDC ACM device, full speed. It connects to Win10 app. The app reads data from the device, they arrive at approx. 500 kB/s. I have a problem that some packets are lost during transfer, mainly when Win10 app is even little busy (e.g. when I move its window - it is GUI app)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used USB sniffer and I can see that during these busy periods sometimes 0xc0010000 (=USBD_STATUS_CANCELED) error occurs on the&amp;nbsp;bulk endoint&amp;nbsp;and then in subsequent packet I can see that some data were lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there to detect this error on MK22F and to retransmit the data? I want the transfer to be 100% reliable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Mar 2017 18:56:23 GMT</pubDate>
    <dc:creator>martindusek</dc:creator>
    <dc:date>2017-03-23T18:56:23Z</dc:date>
    <item>
      <title>Kinetis SDK USB abort</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Kinetis-SDK-USB-abort/m-p/612266#M6343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on MK22F I run USB CDC ACM device, full speed. It connects to Win10 app. The app reads data from the device, they arrive at approx. 500 kB/s. I have a problem that some packets are lost during transfer, mainly when Win10 app is even little busy (e.g. when I move its window - it is GUI app)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used USB sniffer and I can see that during these busy periods sometimes 0xc0010000 (=USBD_STATUS_CANCELED) error occurs on the&amp;nbsp;bulk endoint&amp;nbsp;and then in subsequent packet I can see that some data were lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there to detect this error on MK22F and to retransmit the data? I want the transfer to be 100% reliable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 18:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Kinetis-SDK-USB-abort/m-p/612266#M6343</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2017-03-23T18:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis SDK USB abort</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Kinetis-SDK-USB-abort/m-p/612267#M6344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I count sent bytes in kUSB_DeviceCdcEventSendResponse event in USB_DeviceCdcVcomCallback. In the callback I can count&amp;nbsp;exactly same number of&amp;nbsp;bytes sent as I send by USB_DeviceCdcAcmSend function. If all bytes were confirmed can I really be sure that the bytes were received by Windows PC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 11:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Kinetis-SDK-USB-abort/m-p/612267#M6344</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2017-03-24T11:04:53Z</dc:date>
    </item>
  </channel>
</rss>