<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Difference between a generated and example project with exact same code</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604858#M6234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working with the FRDM-KV10Z board. I am using the KSDK project generator to start playing with it. I also downloaded the KSDK 2.0 to get some examples.&lt;/P&gt;&lt;P&gt;The thing is that when I use the example for the pwm generator (called ftm_simple_pwm) I can build it and I see the blue led of the board dimming as it should. However, if I copy the the same code and add it into my generated project (it has all the drivers already) I can build it but the led does not react. I added breakpoints in the code just in case and it is following it as it should. I am debugging with UART as well and this one works for both cases.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Kinetis Design Studio in a Windows 10 (I know the project generator is tested in windows 7). I have also tried to generate the projects with the advanced settings and even with both x64 and x86 executables (I know my machine is x64). Does anybody have a clue what could be the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jan 2017 13:55:01 GMT</pubDate>
    <dc:creator>borjaserra</dc:creator>
    <dc:date>2017-01-10T13:55:01Z</dc:date>
    <item>
      <title>Difference between a generated and example project with exact same code</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604858#M6234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working with the FRDM-KV10Z board. I am using the KSDK project generator to start playing with it. I also downloaded the KSDK 2.0 to get some examples.&lt;/P&gt;&lt;P&gt;The thing is that when I use the example for the pwm generator (called ftm_simple_pwm) I can build it and I see the blue led of the board dimming as it should. However, if I copy the the same code and add it into my generated project (it has all the drivers already) I can build it but the led does not react. I added breakpoints in the code just in case and it is following it as it should. I am debugging with UART as well and this one works for both cases.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Kinetis Design Studio in a Windows 10 (I know the project generator is tested in windows 7). I have also tried to generate the projects with the advanced settings and even with both x64 and x86 executables (I know my machine is x64). Does anybody have a clue what could be the reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 13:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604858#M6234</guid>
      <dc:creator>borjaserra</dc:creator>
      <dc:date>2017-01-10T13:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between a generated and example project with exact same code</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604859#M6235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the mistake. Silly thing. The pin_mux.c was different meaning that my generated project didn't have the initialization for the blue led. I needed to enable the clock for port D and state that I am using the FTM0 alternative. Then it worked :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 16:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604859#M6235</guid>
      <dc:creator>borjaserra</dc:creator>
      <dc:date>2017-01-10T16:13:49Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between a generated and example project with exact same code</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604860#M6236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;do you know, the "SDK example project cloning"&amp;nbsp;functionality is provided in KDS directly under &lt;EM&gt;main manu - New - Project for Kinetis SDK 2.x&lt;/EM&gt;?&lt;/P&gt;&lt;P&gt;Please ensure your KDS is updated from KDS update site.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 08:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Difference-between-a-generated-and-example-project-with-exact/m-p/604860#M6236</guid>
      <dc:creator>MarekTrmac</dc:creator>
      <dc:date>2017-01-11T08:13:28Z</dc:date>
    </item>
  </channel>
</rss>