<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: eDMA ScatterGatter</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360619#M617</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ole Asbjorn Fadum,&lt;/P&gt;&lt;P&gt;Unfortunately, there's no demo that integrate with ScatterGatter function in SDK now.&lt;/P&gt;&lt;P&gt;However I can share a demo which using the eDMA ScatterGatter feature to transfer the data to external flash through the SPI interface.&lt;/P&gt;&lt;P&gt;The demo was created for another customer in a few month ago and the original demo spi_demo is from the TWR-K60D100M sample code KINETIS512_V2_SC,&lt;/P&gt;&lt;P&gt;you should use the spi_demo.c and isr.h in the SPI_DMA_TEST_Scenario2_scatter_gather file instead of the these files in the original demo, it's done.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2015 09:20:18 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-01-23T09:20:18Z</dc:date>
    <item>
      <title>eDMA ScatterGatter</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360618#M616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KDS-2.0.0 and KSDK-1.1.0.&lt;/P&gt;&lt;P&gt;I need to run a DMA transfer for one cycle, and think of using EDMA_DRV_ConfigScatterGatherTransfer()&lt;/P&gt;&lt;P&gt;with a list of only one destination (source is I2S device).&lt;/P&gt;&lt;P&gt;Unfortunately there doesn't seem to be any example for this, is there anyone which have a sample to provide?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 15:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360618#M616</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2015-01-20T15:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: eDMA ScatterGatter</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360619#M617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ole Asbjorn Fadum,&lt;/P&gt;&lt;P&gt;Unfortunately, there's no demo that integrate with ScatterGatter function in SDK now.&lt;/P&gt;&lt;P&gt;However I can share a demo which using the eDMA ScatterGatter feature to transfer the data to external flash through the SPI interface.&lt;/P&gt;&lt;P&gt;The demo was created for another customer in a few month ago and the original demo spi_demo is from the TWR-K60D100M sample code KINETIS512_V2_SC,&lt;/P&gt;&lt;P&gt;you should use the spi_demo.c and isr.h in the SPI_DMA_TEST_Scenario2_scatter_gather file instead of the these files in the original demo, it's done.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 09:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360619#M617</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-23T09:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: eDMA ScatterGatter</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360620#M618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I'm trying to work with KSDK so the register -&amp;gt; API mapping must be done of course, but it's a start.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jan 2015 07:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/eDMA-ScatterGatter/m-p/360620#M618</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2015-01-26T07:41:28Z</dc:date>
    </item>
  </channel>
</rss>