<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: Serial port at high speed using UART_DRV</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600648#M6139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Hector,&lt;/P&gt;&lt;P&gt;Regarding your issue that you can not communicate successfully with above 115200 baudrate, I think the uart driving clock dismatch with PC leads to the issue. For example, if you communicate between two SCI on the same chip, you can use high baudrate.&lt;/P&gt;&lt;P&gt;I suppose that you communicate between PC and FRDM-K64F, and the PC has precious baudrate. I suggest you use external clock source or crystal and use PLL to get the core/system clock. For the detailed inf about the dismatch of SCI baudrate clock, I suggest you refer to section 52.4.2.9 Baud rate tolerance in the reference manual of K64.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Sep 2016 03:05:12 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-09-09T03:05:12Z</dc:date>
    <item>
      <title>Serial port at high speed using UART_DRV</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600647#M6138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone. I'm using a FRDM-K64F. I would like to use a UART in a high speed mode. I need to transmit/receive data faster than 115200. I tried up to 115200 without problems but faster than that I couldn't do it. I lost characters, I received wrong characters and so on. I need to make a project using RTCS, USB and Serial ports. My code is based on the Ethernet to Serial port example. but it is using a serial port with the "old" nio driver. I migrated the example to the new "UART_DRV" and it is working worse than before. I made a protocol which use different layers, but I can't do the next step if the serial port layer don't work. I configured the serial port using PE and then I send this configuration to my layer through a specific struct for this.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This two tasks which have the same priority are working all the time. This code works until I change the baud-rate from 115200 to 256000, and I want it to run faster than that.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;p&amp;gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void LayerUSART_rx_task (os_task_param_t task_init_data)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SLayerUsartConfigPtr config;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uart_status_t state;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint8_t * buffer;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Waiting until the initialization process is finished */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while(!_LwSemInit.VALID)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;OSA_TimeDelay(UART_RX_BUFFER_TIMEOUT * 5);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;OSA_SemaWait(&amp;amp;_LwSemInit, OSA_WAIT_FOREVER);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;OSA_SemaDestroy(&amp;amp;_LwSemInit);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;_Rx_Buffers_last = _Rx_Buffers_index = 0;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Endless loop for reading from serial&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while(1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;config = (SLayerUsartConfigPtr)_LayerUsart.configLayerStruct;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;buffer = &amp;amp;(_Rx_Buffers[_Rx_Buffers_index][0]);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Wait to receive input data&lt;BR /&gt;#ifdef USART_DMA&lt;BR /&gt;&lt;SPAN style="color: #999999; font-size: 13px;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;state = UART_DRV_EdmaReceiveDataBlocking(config-&amp;gt;instance, buffer, UART_RX_BUFFER_SIZE, &lt;/SPAN&gt;UART_RX_BUFFER_TIMEOUT);&lt;BR /&gt;#else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;state = UART_DRV_ReceiveDataBlocking(config-&amp;gt;instance, buffer, UART_RX_BUFFER_SIZE, UART_RX_BUFFER_TIMEOUT);&lt;BR /&gt;#endif&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kStatus_UART_Success == state)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_Rx_Received = UART_RX_BUFFER_SIZE;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;if(kStatus_UART_Timeout == state)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint32_t bytesRemaining;&lt;BR /&gt;#ifdef USART_DMA&lt;BR /&gt;&amp;nbsp;&lt;SPAN style="color: #999999; font-size: 13px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;UART_DRV_EdmaGetReceiveStatus(config-&amp;gt;instance, &amp;amp;bytesRemaining);&lt;/SPAN&gt;&lt;BR /&gt;#else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;UART_DRV_GetReceiveStatus(config-&amp;gt;instance, &amp;amp;bytesRemaining);&lt;BR /&gt;#endif&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_Rx_Received =&amp;nbsp; UART_RX_BUFFER_SIZE - bytesRemaining;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Error handling */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if((_Rx_Received) &amp;amp;&amp;amp; (_Rx_Received &amp;lt;= UART_RX_BUFFER_SIZE))&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_Rx_Buffers_last = _Rx_Buffers_index;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_Rx_Buffers_index = ((_Rx_Buffers_index + 1) % UART_RX_BUFFER_DEEP);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_SemaPost(&amp;amp;_LwSemReceived);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;void LayerUSART_rx_completed_task (os_task_param_t task_init_data)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint8_t * buffer;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Waiting until the initialization process is finished */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while(!_LwSemReceived.VALID)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;OSA_TimeDelay(UART_RX_BUFFER_TIMEOUT * 5);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Endless loop for processing data read from serial&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while(1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;OSA_SemaWait(&amp;amp;_LwSemReceived, OSA_WAIT_FOREVER);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;buffer = &amp;amp;(_Rx_Buffers[_Rx_Buffers_last][0]);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#ifdef LAYER_USART_ECHO&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LayerUSART_Send(buffer, _Rx_Received);&lt;BR /&gt;#else&lt;BR /&gt;&lt;SPAN style="color: #999999; font-size: 13px;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;LayerUSART_Receive(buffer, _Rx_Received);&lt;/SPAN&gt;&lt;BR /&gt;#endif&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uint8_t LayerUSART_Send(uint8_t * data, uint16_t length)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;uint8_t retval = 1;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if((data != NULL) &amp;amp;&amp;amp; (length &amp;gt; 0))&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;if(LayerUSART_ReadyToSend())&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;uart_status_t state;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;SLayerUsartConfigPtr config = (SLayerUsartConfigPtr)_LayerUsart.configLayerStruct;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#ifdef USART_DMA&lt;BR /&gt;&lt;SPAN style="color: #999999; font-size: 13px;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;state = UART_DRV_EdmaSendData(config-&amp;gt;instance, data, length);&lt;/SPAN&gt;&lt;BR /&gt;#else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;state = UART_DRV_SendData(config-&amp;gt;instance, data, length);&lt;BR /&gt;#endif&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;if(kStatus_UART_Success == state)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;retval = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;return (retval);&lt;BR /&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;/p&amp;gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is an example when I try to make an echo at 256000 bps in a terminal.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;[TX] - &amp;lt;ECHO_*_TEST&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;[RX] - &amp;lt;ECHO_*_TEST&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;[TX] - &amp;lt;ECHO_*_TEST&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;[RX] - ¼Q(êê¥úQ MQò&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;[TX] - &amp;lt;ECHO_*_TEST&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #ff0000;"&gt;[RX] - &amp;lt;ECHO_*_TEST¾&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope you can help me. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 12:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600647#M6138</guid>
      <dc:creator>hectorgastaminz</dc:creator>
      <dc:date>2016-09-08T12:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: Serial port at high speed using UART_DRV</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600648#M6139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Hector,&lt;/P&gt;&lt;P&gt;Regarding your issue that you can not communicate successfully with above 115200 baudrate, I think the uart driving clock dismatch with PC leads to the issue. For example, if you communicate between two SCI on the same chip, you can use high baudrate.&lt;/P&gt;&lt;P&gt;I suppose that you communicate between PC and FRDM-K64F, and the PC has precious baudrate. I suggest you use external clock source or crystal and use PLL to get the core/system clock. For the detailed inf about the dismatch of SCI baudrate clock, I suggest you refer to section 52.4.2.9 Baud rate tolerance in the reference manual of K64.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 03:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600648#M6139</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-09T03:05:12Z</dc:date>
    </item>
    <item>
      <title>Re: Serial port at high speed using UART_DRV</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600649#M6140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have adjusted the system clock using this information&amp;nbsp;&lt;A href="https://www.element14.com/community/community/designcenter/kinetis_kl2_freedom_board/blog/2014/07/15/frdm-k64f-at-maximum-speed-of-120-mhz"&gt;frdm-k64f-at-maximum-speed-of-120-mhz&lt;/A&gt;. I've supposed that my PC hasn't a precious baud-rate, so I calculated different baud-rates and its errors; then I tried with many of them. Now its working at 500000bps and 1000000bps without problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 19:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Serial-port-at-high-speed-using-UART-DRV/m-p/600649#M6140</guid>
      <dc:creator>hectorgastaminz</dc:creator>
      <dc:date>2016-09-29T19:18:28Z</dc:date>
    </item>
  </channel>
</rss>