<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: Connect and DHCP IP</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591918#M5998</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This message is received once PHY is initialized and cable detection is performed. In ethernetif.c file you can find the low_level_init function in which a while loop is waiting until activity on the PHY is received, if no activity is received a "timeout error" will be shown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Be sure that cable is connected correctly and also that you are initializing Ethernet/PHY pins in the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also didn't see any call to lwip_init(); before netif_add function is being called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jul 2016 22:46:17 GMT</pubDate>
    <dc:creator>isaacavila</dc:creator>
    <dc:date>2016-07-25T22:46:17Z</dc:date>
    <item>
      <title>Connect and DHCP IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591917#M5997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to implement very simple function, let's name it connect_and_get_ip(void);&lt;/P&gt;&lt;P&gt;For now I have following code:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;&amp;nbsp;&amp;nbsp; struct netif fsl_netif0; &amp;nbsp;&amp;nbsp; ip_addr_t fsl_netif0_ipaddr, fsl_netif0_netmask, fsl_netif0_gw;&amp;nbsp; void connect_and_get_ip(void) { // Setup IP Config for DHCP ... &amp;nbsp;&amp;nbsp; IP4_ADDR(&amp;amp;fsl_netif0_ipaddr, 0,0,0,0); &amp;nbsp;&amp;nbsp; IP4_ADDR(&amp;amp;fsl_netif0_netmask, 0,0,0,0); &amp;nbsp;&amp;nbsp; IP4_ADDR(&amp;amp;fsl_netif0_gw, 0,0,0,0);&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; /* Add a network interface to the list of lwIP netifs. */ &amp;nbsp;&amp;nbsp; netif_add(&amp;amp;fsl_netif0, &amp;amp;fsl_netif0_ipaddr, &amp;amp;fsl_netif0_netmask, &amp;amp;fsl_netif0_gw, NULL, ethernetif_init, ethernet_input); &amp;nbsp;&amp;nbsp; /* Set the network interface as the default network interface. */ &amp;nbsp;&amp;nbsp; netif_set_default(&amp;amp;fsl_netif0); &amp;nbsp;&amp;nbsp; /* obtain the IP address, default gateway and subnet mask by using DHCP*/ &amp;nbsp;&amp;nbsp; dhcp_start(&amp;amp;fsl_netif0); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("got IP Address!"); &amp;nbsp;&amp;nbsp; // Make it active ... &amp;nbsp;&amp;nbsp; netif_set_up(&amp;amp;fsl_netif0); &amp;nbsp;&amp;nbsp; printf("%s : Interface is up : %d\n", __FUNCTION__, fsl_netif0.dhcp-&amp;gt;state); &amp;nbsp;&amp;nbsp; printf("%s : IP %s\n", __FUNCTION__, ipaddr_ntoa(&amp;amp;fsl_netif0.ip_addr)); &amp;nbsp;&amp;nbsp; printf("%s : NM %s\n", __FUNCTION__, ipaddr_ntoa(&amp;amp;fsl_netif0.netmask)); &amp;nbsp;&amp;nbsp; printf("%s : GW %s\n", __FUNCTION__, ipaddr_ntoa(&amp;amp;fsl_netif0.gw)); }&amp;nbsp; int main(void) {&amp;nbsp; /* Disable the mpu */ &amp;nbsp;&amp;nbsp; MPU_Type *base = MPU; &amp;nbsp;&amp;nbsp; base-&amp;gt;CESR &amp;amp;= ~MPU_CESR_VLD_MASK; &amp;nbsp;&amp;nbsp; /* Init board hardware. */ &amp;nbsp;&amp;nbsp; BOARD_InitPins(); &amp;nbsp;&amp;nbsp; BOARD_BootClockRUN(); &amp;nbsp;&amp;nbsp; BOARD_InitDebugConsole(); connect_and_get_ip(); prox_agent_init();&amp;nbsp; &amp;nbsp; for(;;) {&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; //not important &amp;nbsp; } }&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately I get "PHY Link down, please check the cable connection." on console. It happens during executing netif_add(...) function.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong. I just simply want to connect to serwer and get IP.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paweł Żydziak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 12:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591917#M5997</guid>
      <dc:creator>pzydziak</dc:creator>
      <dc:date>2016-07-20T12:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: Connect and DHCP IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591918#M5998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This message is received once PHY is initialized and cable detection is performed. In ethernetif.c file you can find the low_level_init function in which a while loop is waiting until activity on the PHY is received, if no activity is received a "timeout error" will be shown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Be sure that cable is connected correctly and also that you are initializing Ethernet/PHY pins in the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also didn't see any call to lwip_init(); before netif_add function is being called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 22:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591918#M5998</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-07-25T22:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: Connect and DHCP IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591919#M5999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you provide me tutorial how to "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; initializing Ethernet/PHY pins in the MCU&lt;/SPAN&gt;". Im pretty new in that stuff. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Paweł&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 05:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591919#M5999</guid>
      <dc:creator>pzydziak</dc:creator>
      <dc:date>2016-07-29T05:09:25Z</dc:date>
    </item>
    <item>
      <title>Re: Connect and DHCP IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591920#M6000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which board are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer to any lwIP example that is located at board folder. For example, I am using lwip_httpsrv_bm_frdmk64f example located at &amp;lt;SDK_2_0_FRDM-K64F&amp;gt;/boards/frdmk64f/demo_apps/lwip/lwip_httpsrv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In FRDM-K64F, PTB0 and PTB1 pins are used as RMII0_MDC and RMII0_MDIO respectively, so they are configured in BOARD_InitPins as follows:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14702349131718756 jive_text_macro" data-hasrefreshed="true" data-renderedposition="215.60000610351562_8_1192_144" jivemacro_uid="_14702349131718756" modifiedtitle="true"&gt;&lt;P&gt;/* Affects PORTB_PCR1 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTB, 1u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; configENET.openDrainEnable = kPORT_OpenDrainEnable;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; configENET.mux = kPORT_MuxAlt4;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; configENET.pullSelect = kPORT_PullUp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Ungate the port clock */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_EnableClock(kCLOCK_PortA);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTB_PCR0 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinConfig(PORTB, 0u, &amp;amp;configENET);&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And PTA12, PTA13, PTA14, PTA5, PTA15, PTA16 and PTA17 are also connected to PHY:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14702352558748358 jive_macro_code jive_text_macro" data-hasrefreshed="true" data-renderedposition="411.5_8_1192_224" jivemacro_uid="_14702352558748358" modifiedtitle="true"&gt;&lt;P&gt;/* Affects PORTA_PCR13 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 13u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR12 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 12u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR14 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 14u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR5 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 5u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR16 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 16u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR17 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 17u, kPORT_MuxAlt4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTA_PCR15 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_SetPinMux(PORTA, 15u, kPORT_MuxAlt4);&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check FRDM-K64F's schematic for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, after BOARD_InitPins, BOARD_BootClockRUN and BOARD_InitDebugConsole function, lwip_init function is being called:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14702353889089458 jive_macro_code jive_text_macro" data-hasrefreshed="true" data-renderedposition="739.2999877929688_8_1192_112" jivemacro_uid="_14702353889089458" modifiedtitle="true"&gt;&lt;P&gt;MPU_Type *base = MPU;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_InitPins();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_BootClockRUN();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_InitDebugConsole();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Disable MPU. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; base-&amp;gt;CESR &amp;amp;= ~MPU_CESR_VLD_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lwip_init();&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2016 14:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Connect-and-DHCP-IP/m-p/591920#M6000</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-08-03T14:43:29Z</dc:date>
    </item>
  </channel>
</rss>